Home audio is evolving rapidly, and the consumer demand for immersive, cinema like sound at home is on the rise. As soundbars have become the central audio hub, adoption is still hampered by setup complexity and rigid speaker layouts. Together with StreamUnlimited , NXP addresses these constraints with a reference implementation that enables effortless setup and customized placement.
Home audio systems continue to evolve to deliver cinema-level immersion without the complexity of a traditional multicomponent setup. Soundbars—increasingly seen as the central speaker in whole home audio solutions—can now deliver the performance once reserved for professional setups and dedicated theater speakers. Connected to local sources and streaming services that feature immersive formats (Dolby Atmos®, DTS:X®, 360 Reality Audio™, MPEGH Audio™), advanced post-processing and higher channel have become the standard.
The Placement Problem
Remote speaker positioning remains one of the most challenging aspects of home audio system setup, with most designs built for fixed and ideally placed speakers. Flexible renderers, such as Dolby Atmos® FlexConnect™, allow wireless speakers to be positioned anywhere as the system adapts immersive rendering to arbitrary layouts and audience position. However, to fully unlock this flexibility, systems must know exactly where each speaker is located in the room. This is where UWB spatial ranging and sensing can be transformative. Combining UWB spatial ranging and sensing, adaptive immersive rendering and modular embedded audio platforms enable the next generation of home audio with effortless setup and complete placement freedom.
Immersive audio is no longer just about sound quality – it’s about intelligence, adaptability and removing setup friction. By working closely with NXP, we’ve built a platform that integrates precise UWB ranging, reliable wireless distribution and a production-ready software stack. For audio OEMs, this means a scalable, low-risk path to flexible remote speaker layouts and faster development of next-gen immersive products.
Clement Arnardi, Technical Manager for Wireless Technologies, StreamUnlimited
A Truly Flexible and Adaptive Rendering Solution
Working together, NXP and StreamUnlimited have created a reference implementation that enables highly scalable, easy to integrate, user friendly home audio systems featuring true placement flexibility. Centered around a soundbar platform based on the StreamUnlimited Stream1955 module and NXP Trimension® SR250 ultra-wideband (UWB) integrated circuit (IC), the reference system connects to wireless speakers (equipped with Trimension SR150 UWB Solution) which can be placed freely within the room, eliminating predefined layout constraints.
What makes UWB so compelling for immersive audio is the combination of precise ranging and radar-based sensing. This spatial awareness allows systems to continuously adapt to real world environments and user behaviour. Paired with technologies like Dolby Atmos FlexConnect, UWB helps create a uniquely responsive listening experience that differentiates next generation home audio products.
Sunil Jogi, Director - UWB Marketing and Product Management NXP Semiconductors
Reference implementation
The Stream1955 module offers a flexible, space-efficient foundation for next generation audio devices. Featuring a compact, high-performance embedded Linux audio compute module designed to power advanced networked audio products, from decoding to rendering it hosts a complete streaming audio stack and audio pipeline.. This provides multi-channel (up to 16) audio I/O using standardized inter-ic sound (I²S) interface.
As an NXP Gold Partner, StreamUnlimited brings deep system expertise and production ready software platforms – learn more by exploring their partner profile .
NXP’s industrial and IoT UWB portfolio brings precise, reliable spatial awareness to modern smart home and audio solutions. The Trimension SR250 combines secure UWB ranging with built-in sensing, allowing devices to detect presence, movement and exact location in a room. The Trimension SR150 focuses on accurate ranging and positioning, measuring distances within a few centimeters and determining direction, making it ideal for devices that need simple but highly reliable location tracking. Together, they enable flexible speaker placement and smarter, more responsive home experiences.
UWB Spatial Ranging and Sensing That Is Key to System Optimization
In home audio systems UWB radar technology enables the best placement of speakers by accurately tracking the listener’s position to create the perfect acoustic sweet spot.
- UWB-based listener and speaker localization: Listener position can either be detected using the Trimension SR250 UWB radar connected to the Stream1955 over serial peripheral interface (SPI), or alternatively through a UWB-enabled smartphone. The Trimension SR250 in the main unit also coordinates and performs distance and angle measurements from multiple Trimension SR150 equipped speakers to quickly build a complete and accurate spatial model
- Wireless audio distribution: Once the system knows the room, the Stream1955 renders up to 12 audio channels, outputting them over I²S to local digital-to-analog converters (DACs) or low-latency wireless transmitters. While Bluetooth® Low Energy (BLE) Audio is available for selected channels, when combined with local rendering higher channel count immersive setups benefit from wireless local area network (WLAN) or frequency shift keying (FSK)-based links, which can deliver around 20 ms latency and support up to eight 48 kHz / 24-bit channels
- Flexible speaker roles: An additional advantage of this setup is its support for distinct roles. This can range from relatively simple immersive satellites (combining an MCU, wireless receiver and Trimension SR150 for localization) to fully autonomous Linux-based Wi-Fi 6E/LE self-contained streaming speakers based on modules like the Stream210 . This flexibility allows mixed speaker configurations that can be used standalone or seamlessly join or form an immersive system
The joint StreamUnlimited–NXP reference implementation highlights how UWB spatial ranging and sensing, adaptive immersive rendering and modular embedded platforms work together to enhance accessibility for immersive audio solutions. With automatic, centimeter-accurate speaker mapping and flexible wireless placement, this approach significantly streamlines the setup process and paves the way for scalable, next-generation home audio products.