Ezurio, an NXP Gold Partner, is a leader in wireless and embedded solutions focused on industrial connectivity. With decades of expertise, Ezurio combines advanced wireless innovation with NXP’s processor technology to deliver reliable, high-performance platforms like the Nitrogen HMI—engineered for long-lasting, connected applications.
Industrial HMIs built to perform, connect, and last.
Discover how Ezurio and NXP are redefining reliable edge interfaces in the official product overview.
Smarter Interfaces for a Connected World
Human Machine Interfaces (HMIs) have evolved far beyond basic touchscreens. In factories and buildings they have become the point where data, connectivity, and Edge AI come together. But as workloads grow so does the demand for reliable performance, robust wireless and long product lifecycles.
Design engineers know the real test of an HMI isn’t day-one performance but how the platform holds up over a decade of production and field use. Instead of asking engineering teams to spend time and resources building a platform from scratch, Ezurio has delivered a production-ready HMI that’s field-tested and backed by long-term availability. For OEMs, it means faster integration, reduced risk, and a reliable path to success.
That’s why Ezurio built the Nitrogen HMI , powered by NXP’s i.MX 8M Plus Application Processors, Nitrogen8M Plus SMARC SoM and Sona NX611™ Wi-Fi 6 + Bluetooth 5.4 module based on NXP’s IW611 chipset. Together, they deliver a drop-in HMI platform ready for real-world challenges.
Ezurio Nitrogen HMI: a production-ready platform built on NXP i.MX 8M Plus applications processor for reliable edge interfaces.
Where Traditional HMIs Fall Short
In factories, HMIs must drive smooth GUIs while processing video from inspection cameras, something many boards can’t handle without lag or frame loss. Wireless reliability often collapses in crowded RF environments, and consumer-grade solutions rarely guarantee 10-plus years of updates and support.
Building automation systems face similar challenges. HMIs need to manage data from hundreds of BACnet/IP and wireless sensors and display it in real time. Low-end MCUs quickly hit their ceiling, and missing features like WPA3 security or secure OTA updates introduce risk.
The Nitrogen HMI Advantage
- Built for Real Workloads: The i.MX 8M Plus applications processor gives engineers the compute headroom to run responsive GUIs, AI inference, and live video simultaneously—without trade-offs
- Wireless That Works Out-of-the-Box: Ezurio’s Sona™ NX611 module with NXP’s IW611 chipset delivers pre-certified Wi-Fi 6 + Bluetooth 5.4 performance optimized for dense industrial and commercial environments
- End Product Regulatory Certification: The Nitrogen HMI already carries key regulatory certifications, eliminating one of the most time-consuming and costly steps in product development
- Ready to Deploy: A rugged, enclosed design with included power supply and cables means teams can prototype on day one and cut months from development. HDMI®, LVDS, MIPI, dual GbE, PCIe, RS-485, and GPIO are all built-in; no add-on boards are required
- U.S. Based Supply Chain and Local Support: Designed, built, and supported in the U.S., helping customers reduce supply chain risk. Ezurio also provides direct access to FAEs and engineering support for design, integration, and long-term maintenance
- Powered by NXP: At the core, NXP’s i.MX 8M Plus processor and IW611 wireless chipset bring proven reliability, long-term availability, and a rich ecosystem of software and security support
Why It Matters
The Nitrogen HMI isn’t a development kit; it’s a purpose-built platform that helps OEMs accelerate design, reduce risk, and deliver reliable connected products faster.
By combining NXP’s processing and wireless leadership with Ezurio’s U.S. based design, regulatory certification, and long-term support, the Nitrogen HMI gives engineers a system they can trust—built to perform, connect, and last.
Start your next project with an HMI that’s already ready. Learn more about the Nitrogen HMI