Author

NXP
At NXP, innovation is always now, but our focus is always the future. Our dedicated team of experts is united by a passion to make everyday life more remarkable through technologies that continually redefine life as we know it.
Are you one of those embedded engineers who operates in a very low-level world of direct register accesses? Or are you in the high-level world where the hardware is highly abstracted and differentiating features get lost?
It’s possible to bridge both of these worlds by leveraging a layered approach with software components and the RTOS. This helps you get the basic software done, leaving you with more time and resources for unique application level software. The end result? Your device will be differentiated from similar ones on the market.
Let’s start with a view of embedded software sliced into layers of functionality. Each layer maps to your application’s requirements. Different aspects of an application can also access multiple layers, from high-level functionality to low-level hardware access.
Lowest layer: the microcontroller
The lowest layer is, of course, the microcontroller hardware itself. The unique features of MCU peripherals open the door for differentiating and compelling applications.
For instance, take the Kinetis K22 and compare it to Kinetis KL03. Because Kinetis K22 uses the Arm Cortex-M4 core with floating point unit and adds crystal-less USB functionality, it’s ideal for the broadest range of applications including sophisticated activity monitors and building control. Kinetis KL03, on the other hand offers ultra low power and smaller physical size making it ideal for the smallest portable, battery-powered applications where stand-by time needs to be measured in months — not days.
Enter the hardware access layer
Each MCU peripheral is controlled through a set of memory-mapped registers that are part of the hardware. Directly above the hardware registers, we introduce a set of register access macros. These macros provide the programmer a consistent interface to accessing registers that is mapped 1-to-1 to the documentation in the hardware reference manual.
Building on the register macros, a hardware access layer (HAL) is added. Multiple register operations are combined into single function calls, and API names are abstracted. The HAL is a powerful layer that gives you the ability to directly access differentiating hardware features, while not having to think in terms of registers and bitfields.
And the peripheral driver layer
On top of the HAL sits the peripheral driver layer. Many developers are familiar with this layer, as it appears in slightly different variants in most applications. The driver layer fully abstracts the hardware into generic terms. For instance, an I2C driver has an API defined in terms of I2C-bus operations.
Sitting next to the driver layer is an optional RTOS, such as MQX RTOS. Drivers need to be aware of an RTOS, if present, in order to have the best performance. Atop the RTOS is middleware, such as USB or TCP/IP stacks, an SMBus driver, a Graphic UI system and so on.
Finally, the embedded application builds on all the layers below it.
So, you can see, it’s possible to bridge both of these worlds by using high-level, abstracted peripheral drivers for parts of your application that do not require special features. This may be typical access to a standard communications bus like SPI, I2C, UART or Ethernet, among many others. For atypical use cases or special performance requirements, you can dive down to the lower-level HAL layer to access unique hardware features. Consider use cases that includes special ADC or DAC features such as automatic triggering from other peripherals, or to enable certain low-power capabilities of the hardware. The two approaches can even be combined for a single type of peripheral, where a high-level driver is used for one ADC instance but the HAL is used for another.
Using a layered approach to software provides the ultimate flexibility for software designers and can significantly improve time to market. The Kinetis software development kit (SDK) is the software solution that enables this type of multi-layered access. The picture below illustrates how the layers are organized to optimize the software solution for the microcontroller.
Tags: Automotive, Technologies
At NXP, innovation is always now, but our focus is always the future. Our dedicated team of experts is united by a passion to make everyday life more remarkable through technologies that continually redefine life as we know it.
February 19, 2020
by NXP
March 23, 2020
June 3, 2020
by Lars Reger