In today's highly interconnected world, the security capabilities of Internet of Things (IoT) devices are more
critical
than ever. As Industrial IoT (IIoT) and smart home technologies continue to advance, ensuring robust security design
is
essential to protect sensitive data and maintain user trust.
This article explores the vital certifications and standards that underpin the security of IIoT and Smart Home
devices including:
- Security Evaluation Standard for IoT Platforms (SESIP)
- Platform Security Architecture (PSA)
- Radio Equipment Directive (EU RED)
- Industrial Cybersecurity Standard (IEC 62443)
- Federal Information Processing Standards (FIPS 140-3)
By understanding and adhering to these certification and compliance requirements, developers can build secure,
reliable and connected products that meet the highest security benchmarks.
1. SESIP
SESIP is a security
evaluation methodology tailored for connected devices. Most relevant SESIP Assurance
Levels for
wireless products are SESIP-2 and SESIP-3.
SESIP Assurance Level 2
SESIP-2 provides a moderate level of assurance. This level involves black-box
penetration
testing, which is the highest level applicable to a closed-source platform. For example, IW610 is
SESIP-2
Certified.
SESIP Assurance Level 3
SESIP Assurance Level 3SESIP-3 offers a substantial level of assurance. This level includes
traditional white-box
vulnerability analysis, structured around a time-limited source code analysis combined with a
time-limited penetration
testing effort. For example, RW612 is SESIP-3
Certified.
Relevance to IIoT and Smart Home
NXP, as a Wi-Fi / Bluetooth / 802.15.4 solutions provider, can showcase SESIP certification to
demonstrate their
connectivity SoCs/IPs meets mandated security functional requirements (SFRs), such as secure boot and
secure
communication.
Device OEMs can reduce their product certification burden by reusing SESIP-certified components.
2. PSA by Arm
PSA
Certified requires strict adherence to the Platform Security Architecture (PSA) as defined by
Arm. PSA
certification
demonstrates robust software isolation, secure boot, cryptographic operations and resistance to basic
attacks.
PSA Certified Level 2
PSA Level 2 provides protection against remote, scalable software attacks and is
suitable for
IoT devices that are unlikely to be under physical attack.
PSA Certified Level 3
PSA Level 3 offers protection against physical attacks as well as software
attacks. This is
ideal for devices that are of higher risk to multiple attack types, such as smart locks and payment
systems.
How PSA Differs from SESIP
While PSA uses the SESIP evaluation methodology, the key difference is that PSA measures compliance with
ARM’s reference
architecture, while SESIP is more flexible in defining the scope of security functions
SESIP is the framework, while PSA is the branding/application from ARM
PSA Certified Level 3 provides protection against physical attacks as well as
software attacks, making it critical for
applications such as smart locks, which are vulnerable to both attack types.
The RW612 Wireless MCU provides differentiated security compliance with both PSA Certified Level 3
and SESIP Level 3. Learn more
about the RW612.
3. EU RED, Article 3 (d/e/f)
The Radio Equipment Directive (RED) specifies essential requirements for radio-enabled devices in the EU,
particularly
under Article 3(3) which focuses on cybersecurity, privacy and fraud prevention.
Starting from August 2025, the following mandatory requirements will be enforced:
Article 3.3 (d) Network protection, aiming to prevent and mitigate attacks over the network.
|
Article 3.3 (e) Privacy protection on all radio equipment capable of processing personal
data. |
Article 3.3 (f) Fraud protection on internet-connected devices with money transfer
capabilities. |
| Access control |
Access control |
Access control |
| Authentication |
Authentication |
Authentication |
| Secure updates |
Secure updates |
Secure updates |
| Secure storage |
Secure storage |
Secure storage |
| Secure communication |
Secure communication |
Secure communication |
| Cryptographic key management |
Cryptographic key management |
Cryptographic key management |
| No known exploitable vulnerabilities |
No known exploitable vulnerabilities |
No known exploitable vulnerabilities |
|
Event logging |
Event logging |
| Best practice cryptography |
Best practice cryptography |
Best practice cryptography |
| Configuration and documentation of network interfaces |
Configuration and documentation of network interfaces |
Configuration and documentation of network interfaces |
| Limit exposure of services via related network interfaces |
Limit exposure of services via related network interfaces |
Limit exposure of services via related network interfaces |
| Input validation |
Input validation |
Input validation |
| Resilience |
Data erasing |
Input validation |
| Traffic control |
User notification |
Equipment integrity |
These requirements aim to enhance the cybersecurity attributes in devices aiming to provide better assurance
and
reliability of radio equipment, making them safer for users and networks alike.
Conformance and Certification:
- Devices will need a conformity assessment (self-declaration or NB involvement)
- Initial evaluation was based on Common Criteria or ETSI EN 303 645 and IEC 62443. EN-18031 is now the
harmonized
benchmark for EU RED compliance
- Connectivity solutions should support the security/cybersecurity capabilities needed by the OEM to meet
RED Article
3(3)
4. IEC 62443
IEC 62443 is a multi-part standard for securing Industrial Automation and Control Systems (IACS), divided
into parts for
components, systems and organizational processes. Chip vendors can certify individual components to IEC
62443-4-2
through labs like TUV, DEKRA.
Relevance to IIoT/Smart Home:
- Critical Infrastructure: Becoming increasingly important for IIoT systems deployed in critical
infrastructure (for example,
smart energy, smart buildings)
- Connectivity Components: Wi-Fi, Bluetooth/BLE, IEEE 802.15.4 must support secure communication,
authentication,
firmware updates and logging features to comply with IEC 62443-4-2 at the system level
5. FIPS 140-3
FIPS 140-3 is the latest version of the Federal Information Processing Standards for cryptographic modules,
succeeding
FIPS 140-2.
- Enhanced security: FIPS 140-3 provides a standardized framework for cryptographic modules, ensuring the
integrity,
confidentiality and availability of sensitive information
- Trust and compliance: Organizations that comply with FIPS 140-3 can build trust with their customers
and partners by
demonstrating their commitment to high-security standards
Cryptographic Algorithm Validation Program (CAVP)
CAVP certifies individual cryptographic algorithms like AES, SHA and ECC. It is a prerequisite for FIPS 140-3
certification. Chip vendors often precertify their cryptographic IP via CAVP before integrating it into a
full
module
for CMVP certification.
Claiming FIPS Support
To claim FIPS support, a module must be listed in the NIST Crypotographic Module Validation Program (CMVP),
which
involves independent testing and lab submission.
Self-Tests for Customers
FIPS-compliant cryptographic libraries used in controllers (for example, Wi-Fi, Bluetooth/BLE, 802.15.4)
perform
self-tests
on
demand to verify integrity and correct cryptographic operations.
Conclusion
Understanding security certifications and standards is crucial for developing secure IIoT and smart home devices.
These
certifications not only bolster the security and reliability of connected products but also foster trust among
consumers
and stakeholders. As the IoT ecosystem continues to evolve, proactively staying ahead of security standards will be
pivotal in safeguarding the future of connected technologies.