With the introduction of Matter, the need for smart home devices to support multiple networks has become more important. Matter, a unified application layer that delivers interoperability across brands and ecosystems, was purposefully designed to enable secure interoperability by building the foundation on the Internet Protocol and to coexist with the millions of smart home devices already in homes today.
A typical smart home network will most likely consist of multiple technologies, as seen in the figure below. For example, there could be battery-powered or power sensitive devices using Zigbee or Matter over Thread and more advanced or always-powered devices using Matter over Wi-Fi.
Visit www.nxp.com/matter to learn more.
For a better viewing experience, download the block diagram.
In this network topology, there is at least one central device ensuring coexistence of the ecosystems by managing and interconnecting these devices. A gateway/hub is typically the optimal device to do these tasks and must embed multiple roles for the smart home local network: Zigbee Coordinator, Thread Border Router, Matter Controller and a Zigbee to Matter bridge. The Dual PAN use cases include:
Dual PAN is a feature that allows devices to participate in two IEEE 802.15.4 personal networks at the same time. Being able to do this enables interoperability of Matter with existing market devices and more intelligent automation, e.g., automatically dimming lights and turning off or pausing appliances during a peak demand of energy.
Determining the most effective way to implement Dual PAN for a given use case entails assessing and prioritizing the requirements and priorities. These include:
NXP performed extensive testing for two architectures to provide context and data to facilitate design decisions. The two architectures evaluated are shown in the figure below. Note that RF Channels A and B in the figure could be the same or different depending on the ecosystem configuration and constraints.
For a better viewing experience, download the block diagram.
With these architectures defined, NXP created two configurations on which to perform the testing.
| 1 Radio Solution | 2 Radio Solution |
|---|---|
| i.MX Linux Host MCX W71 (Thread and Zigbee) |
i.MX Linux Host K32W0 (Zigbee) + IW612 (Thread) |
A comprehensive application note is available to provide details on the test setup, the tests run, the data collected and the takeaways.
As mentioned earlier, each device's role in the network contributes to the Dual PAN results. The devices can be sleepy or mains-powered (where the radio is always listening) and networks can use the same or different RF channels. Dual PAN use cases typically involve two routing (always on) devices.
| Network 1 | Network 2 |
|---|---|
| Sleepy | Sleepy |
| Routing | Sleepy |
| Sleepy | Routing |
Routing |
Routing |
For a better viewing experience, download the block diagram.
Dual PAN can be architected as a single or dual radio solution depending on the intended use case and priority of the requirements. These requirements include quality-of-service (network performance), role of device(s) on each network, ownership and control of each network and system cost. Overall, the data demonstrates that there is a significant improvement for error packet loss and latency observed in a dual radio architecture, especially when there is a higher payload size and increased RF activity.
NXP's comprehensive portfolio provides solutions for the various Dual PAN use cases which have different requirements for processing and networking. The table below provides a snapshot of NXP's system-level solutions per application and use case.
| Applications and Use Cases | Single Radio Solution | Dual Radio Solution |
|---|---|---|
IoT HubZigbee Coordinator, Thread Border Router, Wi-Fi, Ethernet, Matter Controller |
Linux Host
i.MX 9 (Matter, Thread Border Router) |
Linux Host
i.MX 9 (Matter, Thread Border Router) RTOS Host |
BridgeMatter Zigbee to Thread Bridge with routing capabilities on both Zigbee and Thread |
Linux Host
i.MX 9 (Matter, Thread Border Router) RTOS HostRW612 (Matter, Thread Border Router, Zigbee Bluetooth LE) |
RTOS Host
RW612 (Matter, Thread Border Router, Zigbee Bluetooth LE) |
As Matter adoption continues to grow, device makers building smart home devices must enable the transformation of the smart home to the intelligent and autonomous home while also ensuring an ease-of-use experience for consumers. This means supporting existing technologies, especially devices already in millions of homes today. NXP understands the complexities involved in creating this seamless experience and remains committed to providing tailored solutions that address the key technology requirements outlined in this article and the associated application note.
Sujata Neidig has over 30 years of experience in the semiconductor industry and is currently Director of Marketing for Wireless Connectivity where she drives product marketing and standards efforts for IoT connectivity. She also represents NXP on the Thread Group and Connectivity Standards Alliance’s Board of Directors as well as serving as Thread Group’s VP of Marketing. She is based in Austin, TX.
Michael Vannier currently as Wireless Product Marketing Manager has over 10 years of experience in software development and system solutions with wireless connectivity. He is currently part of NXP's product marketing team where he drives product and software requirements and definitions for wireless MCUs.