Video networks are no longer just watching the world — they’re helping shape it. In hospitals, retail stores, factories and cities, surveillance systems are evolving into intelligent edge systems that analyze data, flag anomalies and help make decisions in real time.
But as these systems grow more autonomous and connected, they also become more vulnerable. Cyber threats are evolving in speed, scale and sophistication, targeting everything from firmware and credentials to the video footage itself. The surveillance industry finds itself at a critical crossroads, where smarter systems demand stronger, embedded trust.
Axis Communications, a pioneer in network video, saw the shift coming early. To stay ahead, they’re bringing security into every layer of their systems — from software to silicon — powered by strategic collaboration with NXP.
What began as a supplier relationship has grown into a long-term collaboration. Together, Axis and NXP are aligning roadmaps, solving complex cybersecurity challenges and stepping forward with a shared vision for secure, intelligent surveillance.
With the rise of AI-driven applications, surveillance has entered a new era — and so have the risks. Systems are now targets for deepfake manipulation, remote intrusion and data tampering. The attack surface is expanding across increasingly connected fleets, cloud integrations and third-party ecosystems.
Meanwhile, compliance requirements are growing just as quickly. Initially driven by the North American market, demand for FIPS 140-3 Level 3, the highest standard for cryptographic hardware security, is accelerating across federal, industrial and critical infrastructure systems, now becoming a globally recognized benchmark. Conversations around post-quantum cryptography (PQC) are also beginning to shape design decisions.
Axis needed hardware that could do more than meet current regulations — it had to scale for the future.
The solution: EdgeLock® IoT Secure Elements. These tamper-resistant chips provide a hardware-based root of trust, protecting cryptographic keys, validating device identities and securing communication channels. With the integration of each new generation of EdgeLock® chip — from the EdgeLock SE050 to the EdgeLock SE051 and now the EdgeLock SE052F — Axis has continued to strengthen its security, building an architecture that keeps pace with evolving threats.
FIPS 140-3 Level 3 certified IoT secure element in the industry: EdgeLock SE052F
Generations of EdgeLock IoT secure elements deployed by Axis
Million Axis IoT devices deployed with NXP EdgeLock IoT secure element
As the collaboration deepened, NXP’s role extended beyond just silicon support, looking at the security aspects of Axis’s entire development cycle by:
This collaboration helped Axis bring a major breakthrough to market: the first FIPS 140-3 Level 3-compliant network camera — a milestone for embedded trust in video surveillance.
While achieving this certification is usually a rigorous process requiring advanced cryptography, full tamper response capabilities and third-party lab validation, the EdgeLock SE052F simplified the path. With pre-certified, hardened security built in, Axis was able to reduce development time, streamline testing and accelerate time to market.
Built on the EdgeLock IoT secure elements, Axis’ latest generations of network products, including cameras, intercoms and speakers, deliver the following capabilities:
Together, these use cases deliver stronger protection and position Axis to meet both today’s compliance demands and tomorrow’s emerging risks.
Explore the EdgeLock SE052F. The EdgeLock SE052F is a ready-to-use platform for secure Industrial IoT operations. Designed as a turnkey solution, it runs cryptographic functionality and is the first hardware secure element certified to the latest version of FIPS 140-3 Level 3. Learn more
Surveillance systems will only become more intelligent and more critical. More devices. More data. More autonomy at the edge. That also means more responsibility to design for trust from the start.
Axis and NXP are looking ahead. With a security mindset and a foundation of collaboration, we’re continuing to provide secure, scalable solutions for what’s next in surveillance, from advanced cryptography to post-quantum resilience.
Together, we’re stepping forward into a more secure and intelligent future.
Axis enables a smarter and safer world by improving security, safety, operational efficiency and business intelligence. As a network technology company and industry leader, Axis offers video surveillance, access control, intercoms and audio solutions. These are enhanced by intelligent analytics applications and supported by high-quality training.
Learn more about Axis CommunicationsWhite Paper Aug 4, 2025
Tags: Industrial, Security, Step Forward, Technologies
Product Manager, NXP Semiconductors
Giuseppe is product manager at NXP Semiconductors. As part of the Industrial IoT and NFC security team, he is driving NXP’s IoT secure element offering for Industrial IoT products making security more accessible. He works with customers and supports them in understanding security threats, cybersecurity trends and helps in the realization of their secure Industrial IoT solution. Giuseppe has experience in system engineering roles with a focus on IoT, edge and cloud architectures, standardizations and cybersecurity.
With more than 20 years’ experience in the semiconductors market, Antje leverages her understanding of security and mass market to drive NXP secure element solutions into the industrial and smart city markets.