Sign in to access this content and additional site features.
This course teaches viewers how to create a CodeWarrior® project that uses Processor Expert® to configure and run the TSS (Touch-Sensing Software) library to detect touch and touch position using the analog slider in the FRDM-KL25Z board. The course also shows how to configure a simple PWM output by configuring the KL25Z TPM module. This PWM output is then used to change the intensity of an LED on the board according to the finger position on the touch analog slider. A minimal amount of code is written as most of the coding is done by Processor Expert®, highlighting the value of this tool in creation of applications.
This tutorial uses the following hardware and software components: