In
my blog last month, I discussed the claims that the National Security Agency (NSA) influenced
software, hardware and semiconductor companies to undermine user privacy and
security by deliberately building vulnerabilities and backdoors into their
products. This month I want to discuss the QorIQ platform security
implementation in light of specific claims
related to the NSA, NIST and random number generators.
Virtually every
PowerQUICC
and
QorIQ
product developed since 2000 has incorporated a security engine (we call it
the SEC) which includes a random number generator. Random numbers are
important inputs to cryptographic key exchange protocols such as IKE (Internet
Key Exchange) and the SSL client-server handshake. If the
‘random’ input to the key exchange protocol isn’t so
random, it is easier for an attacker to guess the value of the key exchanged
via an otherwise strong protocol, thereby allowing eavesdropping of an
encrypted communications session.
Random number generator is an imprecise term; it doesn’t tell you
anything about the source of the randomness. More precise terms are TRNG
(‘true’ random number generator) and PRNG
(‘pseudo’ random number generator).
TRNGs are entropy sources, amplifying the uncertainty in the analog world to
create a digital value. Attackers attempt to control physical variables
(voltage, temperature, external timing, transistor manufacturing) to cause
TRNGs to produce lower entropy values.
PRNGs, aka DRBGs (deterministic random bit generators), are
cryptography’s great oxymoron. Their outputs are completely
deterministic, if you know the algorithm used and the starting value, called a
seed. Even if the attacker knows the DRBG algorithm, so long as the seed
remains a secret, the subsequent outputs appear totally random. Wonderful, but
why use a ‘deterministic’ RNG when true RNGs exist? For
starters, when NIST certification is required!
The US National Institute of Standards & Technology is responsible for
validating cryptographic implementations. Prior to 2004, NIST didn’t
have a standard for certification of random number generators. They offered
what were effectively ‘best practices’ for statistical
evaluation of a TRNG’s output, but statistical evidence wasn’t
sufficient for NIST to certify that a TRNG always generated unpredictable
outputs. Last decade, NIST began issuing certificates for PRNGs and more
recently DRBGs. PRNGs & DRBGs are easy to test and certify; NIST gives you
a seed value, and you give them a few MBs of random numbers generated from the
seed, demonstrating that you’ve applied the deterministic algorithm
properly.
In addition to certifiability, PRNGs/DRBGs are used because they can have
significant performance advantages over TRNGs. When a security protocol like
IPsec needs 16B of random Initialization Vector per packet, and you need to
support millions of packets per second, it takes a PRNG/DRBG to keep up. For
this reason, RNGs on PowerQUICC and QorIQ processors combine TRNG with PRNG or
DRBG. External seeds are accepted for testing purposes, but operationally, the
TRNG initially (and periodically afterward) creates a high entropy seed for
the high-speed deterministic portion.
What then are the most recent claims regarding NSA, NIST and US companies? As
mentioned above, PRNGs and DRBGs use cryptographic algorithms, not analog
inputs, to generate their outputs. NIST specifies several acceptable
algorithms for DRBGs, including hashes, HMACs, block ciphers and asymmetric
encryption based on elliptic curve cryptography. This last method,
specifically the Dual Elliptic Curve DRBG, has been discovered to leak
information which attackers can use to determine the future outputs of the
DRBG.
Suspicions were raised about Dual EC even prior to its standardization, leading some to conclude NIST either cooperated knowingly with the NSA to
push a flawed standard or NIST lacks the independent knowledge of
cryptography to evaluate algorithms. It seems either way, NIST’s
international standing as a non-political technical resource for crypto
standards development has been tarnished.
The dust from the fielding of this flawed standard has yet to settle. Software
implementations need to be located and patched. Fortunately there
doesn’t seem to be any instance of a major silicon vendor implementing
Dual EC as their integrated RNG engine. It won’t be easy, but Dual EC
can be rooted out of software products; replacing fielded silicon would be
cost prohibitive.
As previously mentioned, we have been integrating RNGs in our processors
before NIST offered a standard to certify against. Our entropy sources are
submitted to 3rd party labs for statistical analysis and design review by 3rd
party labs. Previous RNGs used SHA-1 for the deterministic portion, our most
recent RNG (RNG4) uses SHA-256 (and its internal TRNG claims full entropy).
Why SHA-256, not Dual EC for the RNG4? Although we’ve integrated
elliptic curve acceleration in our SEC engines from the beginning, it is an
algorithm we hesitate to offer for more than public key. ECC has a history of
intellectual property rights ambiguity, many permutations and overall seems
less studied than the alternatives. As a DRBG algorithm, it is far slower than
hash, HMAC or block cipher alternatives. Conversely, at the time we selected
it, SHA-256 had just survived considerable scrutiny
following reports of success in attacking reduced rounds of SHA-1, and we knew it would support our key exchange and random IV performance
requirements.
Our conservative choice in a SHA-256 DRBG implementation doesn’t mean
we believe cryptography should sit still. New algorithms do need to be
invented, but they should only be standardized after they are competitively
analyzed in a highly transparent process. NIST committing to such a course of
action is one way it can restore its reputation as an honest broker.
Do our efforts to take our crypto accelerator implementations through
NIST certification still provide value to our customers? We believe so. When
the value of the algorithm itself isn’t in question, NIST certification
proves the correctness of our implementation, which assures interoperability
as well. When our implementations are certified, our customers can leverage
our certificates and avoid repeating those tests at a system level.