Established companies and emerging start-ups are putting a stake in the
Internet of Things ground, an opportunity with estimates of 50 billion devices
connected by 2020.
Standing in the way for many companies is the increasing complexity of
technology inside connected devices. Shortened design cycles further fuel
pressure felt by designers — the shelf-life of an IoT device is
similar to a smartphone, from 12 to 18 months. If your new or updated product
isn’t first out the door, another product will take its place.
Getting an idea hatched into a working prototype isn’t always easy,
regardless of design experience. Where do you start, especially if
you’re a start-up with limited resources?
It’s not just the chip – it’s about the
support
Today, the most important factor in deciding what processor you base a design
on isn’t the chip itself. It’s about the ecosystem that supports
it.
With the announcement of the i.MX 7 series, we’re announcing an
ecosystem of partners to help you bring your designs to market without delay.
(Read about the
i.MX 7 series highly integrated multi-market applications
processor
for secure and portable IoT devices that utilizes both the ARM®
Cortex®-A7 and Cortex-M4 cores to enable Heterogeneous Multicore
Processing. )
Full speed ahead to your IoT device
NXP offers the general-purpose i.MX 7 SABRE development board and the
WaRP7 wearable reference design
board accelerates wearable product development. However, the majority of our
development ecosystem is delivered through our partners.
We’ve worked with six companies to deliver evaluation boards (which
will be on display at our Embedded World booth) aimed at the
different target markets of the i.MX 7 series.
Phytec accelerates a range of embedded applications (IoT gateways,
factory/ building automation, machine vision) with the
phyCORE®-i.MX7 System on Module (SOM)
as a drop-in CPU solution, as well as the
phyBOARD-i.MX7 Zeta Single Board Computer (SBC). The
Zeta SBC is a two-PCB counterpart to the phyCORE-i.MX7 SOM and provides
a development kit that breaks out major interface signal to
plug-and-play or pin-level connectors. Both boards support Linux.
Toradex’s
Colibri iMX7D 512MB
and
Colibri iMX7S 256MB
use the i.MX 7Dual and i.MX 7Solo respectively. These highly efficient
yet powerful modules offer advanced security features in a small SODIMM
form factor. They’re well integrated into an extensive ecosystem,
allowing customers to start immediate application development. Both
Linux and Windows Embedded Compact are supported.
The
Nitrogen7 board
from Boundary Devices provides a standalone evaluation
platform or a production-ready single-board computer. It runs
Linux, has a direct interface to a resistive touch display and has
integrated Qt 5.5. This allows for quick development of a user interface
and makes it ideal for HMI.
The
PICO-IMX7-EMMC
from Technexion is a small footprint SOM equipped with
a wide array of high-speed connectivity engineered to support IoT
endpoints, wearable applications, appliances, drones or industrial
mobile terminals.
The
NOVPEK™i.MX7
from Novtech Inc. targets platform engineering by
providing access to all i.MX 7 features. This enables system architects
to create an intended system in a matter of days, hardware engineers to
verify each combination of IOMUX and software engineers to start
developing code early in the cycle.
The Arrow i.MX 7Dual 96Boards Consumer Edition is the
first Arm Cortex-A7 board in the 96Boards Consumer Edition form factor.
The i.MX 7 HMP architecture is an ideal fit with the low and high-speed
expansion connectors of the 96Boards CE design. These features (combined
with the growing eco-system of 96Boards mezzanine cards) enablerapid
prototyping of smart home, building automation and portable
instrumentation.
Tools & Software Partners
Once you’ve selected an i.MX 7 board, what development and debug tool
are you going to use? NXP worked with Arm to enable
simultaneous multicore Cortex-A and Cortex-M system debug and trace with
Arm DS-5
development and debug tool. This allows developers to fully utilize the HMP
architecture without slowing down development.
Utilizing both the Cortex A and M cores might require software expertise, NXP
engaged early with several partners to provide support tools and services.
-
Adeneo Embedded
developed a demo that focuses on the i.MX 7’s power management
capabilities (on-view at NXP’s Embedded World booth). Cycling through
the different system power states of the shared Linux/FreeRTOS environment,
Adeneo shows the full potential of the heterogeneous Cortex-A and Cortex-M
core environment. They’re an official NXP partner for Linux, Android,
QNX and Windows Embedded development on i.MX architectures.
If you’re familiar with Linux development on a Cortex-A core, the
Cortex-M core offers potential for new low-power modes. It may, however, prove
a challenge for those that require more than our Free RTOS. To help you fully
explore the potential of both cores, NXP worked with Micrium and Prove &
Run for specific usage models.
-
Micrium’s
µC/OS
RTOS delivers kernel and connectivity solutions running on both cores. The
µC/OS kernels, TCP/IP, CAN, USB and File System stacks have all been
ported to the i.MX 7. OpenAMP support is also available. Micrium offers
high performance with increased power efficiency while lowering
BOM costs due to reduced memory resource usage.
-
Prove & Run’s
ProvenCore
is an ultra-secure OS kernel down to the generated code. ProvenCore can
be used to build a security perimeter around your preferred
OS—providing an unmatched level of defense against hackers.
Once you decide on operating systems, you might want work on how to show the
data collected through an effective graphical user interface.
-
Some of our aforementioned partners (Boundary Devices, Adeneo) offer
integrated solutions with
Qt, a cross-platform application framework.
-
If the need is to design a rich, high-performance GUI on a short timeline,
then
Crank Software’s Storyboard Suite is an
excellent choice (we’ll be showing an i.MX 7 smart home solution
developed by Crank at our Embedded World booth).
Maybe you’re still not sure where to start. The answer then might be
expert advice through technical training.
HandsOn Training
is both an Arm Authorized Training Center and an NXP Training Proven Partner.
We’ve worked with them to develop the – Designing with the i.MX 7 Family
training program. And like the rest of our i.MX 7 ecosystem, it’s
available now.
Want to see all of this is action, with a variety of demos aimed at the
different i.MX 7 usage models? Then visit the NXP booth (4A-220) at Embedded
World in Nuremberg, Germany February 23-25, 2016.