The automotive market is changing rapidly driven by the revolution that is
turning vehicles from mechanical machines into connected, electric robots,
where passengers can relax and be entertained while being driven to their
destination.
Such epochal change has deep impact on all aspects of the vehicle, from the
number of ECUs (electronic control unit) and their compute power to the
complexity of how they are interconnected, and from how these systems are kept
safe and secure from external hackers and internal bugs. Arguably though,
software is going through the biggest change of all.
Today’s automotive software dictates the user experience much more than in the
past. Software defines how fast and far a car can go, how connected and
entertained the passenger can be, and in the end, determines the vehicle’s
value.
In this new world, NXP is positioned to offer platform solutions that can
enable OEMs and Tier-1s to first define and then deploy new software-defined
products. The new SJA1110 Ethernet switch plays a key role in such reference
designs.
NXP Connected Gateway System Solution
The gateway has a critical role in the vehicle. It is in fact this ECU that
interconnects, manages and updates all other ECUs in the vehicle. It also acts
as interface to the external world by securely communicating with the cloud.
GoldBox is NXP’s system solution targeting connected, service-oriented gateway
applications. It is built around NXP’s S32G Vehicle Network Processor and the
new 10-port Ethernet switch (SJA1110) and uses 15 unique, and 35 total, NXP
components. Additionally, GoldBox leverages the capabilities of NXP’s VR5510
power management IC (PMIC) that powers the whole system. What makes this
automotive-grade solution so special is that it integrates all the necessary
hardware capabilities and basic software layers to accelerate customers’
production ECU development efforts. Additionally, the NXP S32 Design Studio
(S32DS) provides a complementary Integrated Development Environment (IDE) for
programming both the SJA1110 Ethernet switch (which also includes an Arm®
Cortex®-M7 core) and the S32G processor with the same graphical user
interface.
NXP creates highly optimized solutions for vehicle networking applications.
How can the
SJA1110 Ethernet switch improve your design?
Going Beyond the IC
The GoldBox reference platform is more than just a solid hardware baseline.
New vehicles will require new concepts to be deployed in the vehicle. GoldBox
helps engineers to develop innovative networking solutions such as:
-
Extended Networking Security
-
By taking advantage of the true strengths of each component, NXP offers
a new concept for securing the data that is being transported by the
in-vehicle network, leveraging a combination of the SJA1110 Ethernet
switch and the S32G processor. Ethernet switches are the main I/O
interfaces for Ethernet data. All Ethernet packets reaching the gateway
go through a switch, so the switch is the ideal place to deploy the
first line of defense and monitoring of data. This is why the SJA1110
comes with such powerful monitoring classification and filtering
capabilities. At the same time, only a processor such as S32G, is fully
aware of the status of the system and can make decisions based on this
knowledge. The combination of the devices offers a strong platform for
advanced Intrusion Detection and Prevention Systems (IDPS). For that
reason, NXP believes that a combination of SJA1110 and S32G, where
security tasks are allocated between the two devices, can bring the
extra advantage that no single device delivers. Customers and partners
using NXP’s GoldBox can leverage these advanced networking security
capabilities to explore new concepts and create truly differentiating
products.
-
Safety
-
Similar to security, safety applications can also take advantage of the
NXP system solution. In an in-vehicle network that is primarily based on
Ethernet, ASIL B rated Ethernet components such as the new SJA1110
Ethernet switch can contribute to extending the safety of the vehicle by
constantly monitoring itself and the cables connected to it. Once a
deviation is detected, the SJA1110 can interact with the ASIL D S32G
processor or the VR5510 PMIC to notify the system and trigger a
potential reaction.
Ethernet based in-vehicle network transporting safety critical information
-
Diagnostics
-
By leveraging the security and safety capabilities of SJA1110 with the
networking and compute power of the S32G, customers can now imagine new
diagnostics possibilities. For example, by combining the diagnostic
information with a service-oriented protocol, customers can deploy a
cloud-based fleet diagnosis system and trigger new mechanisms for
predictive maintenance. GoldBox comes with the basic software building
blocks that enable customers to experience just this.
-
Efficiency (TC10)
-
For an in-vehicle network that is primarily based on Ethernet and
running on batteries, energy efficiency is paramount. All NXP Ethernet
components support a new, standardized wake up mechanism, commonly
referred to as “TC10 wake up mechanism”. GoldBox includes the necessary
hardware building blocks and on-board circuitry to deploy this mechanism
in a TC10-enabled network, therefore taking full advantage of this new
capability.
-
Time-Sensitive Networking (TSN)
-
Upcoming in-vehicle networking will merge critical and non-critical
traffic on the same wires. TSN is a standardized set of tools which
enables just this: ensuring that critical traffic is delivered on time
whilst also supporting less critical data in the same network. Both
SJA1110 and S32G implement the most relevant TSN standards for the
automotive use-case. GoldBox is then the ideal platform to first
evaluate these solutions and then build on top of these to develop new
applications that can take advantage of TSN capabilities.