Getting Started with the EVBMA6X02BMU Evaluation Board

Last Modified: Sep 18, 2025Supports Optimized Battery Management Unit with BMA6X02

Contents of this document

  • 1

    Out of the Box
  • 2

    Get to Know the Hardware
  • 3

    Configure Hardware
  • 4

    Install Software

1. Out of the Box

The EVBMA6X02BMU is an evaluation board composed of all necessary headers, jumpers and signal test points to quickly evaluate NXP products.

This document is intended to help a user quickly set up, configure, and operate the EVBMA6X02BMU evaluation board.

1.1 Kit Contents and Packing List

The kit contents include:

  • EVBMA6X02BMU - optimized battery management unit
  • Power supply (12 V)
  • Cable for supply and CAN interface
  • ETPL cable - two-wire twisted pair TPL cable (50 cm)
  • 3.3 V FTDI cable

1.2 Additional Hardware

In addition to the kit contents, the following hardware is necessary or beneficial when working with this board.

  • Power cord to connect the power supply to the grid
  • Additional AFE boards (for example, EVBMA7118 or EVBMA777T2) that should be controlled by the EVBMA6X02BMU board
  • PC with programming environment for the S32K358 and associated debug probes

2. Get to Know the Hardware

2.1 Board Features

  • MCU (S32K358)
  • SBC (FS26)
  • Communication gateway (BMA6X02S)

2.2 Board Description

The key components are listed in Table 1.

Component Description
U43 - FS2633D SBC to generate the supplies for all components on the board
U31 - S32K358 MCU to control the board
U402 - BMA6X02S GTW to allow communication to the other boards of the battery management systems
U20 - TJA1145A CAN transceiver to allow communication to other CAN devices

Figure 1. EVBMA6X02BMU Overview

Figure 1. EVBMA6X02BMU Overview

3. Configure Hardware

The EVBMA6X02BMU has several configuration options. The most important ones are the clock and SPI configuration of the BMA6X02S.

3.1 Clock Configuration

The BMA6X02S has three clock configuration options. It can operate with an internal clock, an external crystal or an external clock source. The default configuration is the external clock source, where it is assumed that the S35K358 is configured to provide this clock to the pin OSCP. The OSCP pin is connected on the board to the pin PTB5_47_CLKOUT_RUN_TP8. A change of the clock source selection can be done with R429, R430, R431 and R432 (see Figure 2). Refer to the BMA6X02S data sheet for details on how to change the configuration.

Figure 2. Clock Configuration of the BMA6X02S

Figure 2. Clock configuration of the BMA6X02S

3.2 SPI Configuration

The BMA6X02S has three SPI configurations. It can operate as a single or a dual SPI with the response SPI as a controller or a target. The default configuration of the EVBMA6X02BMU is the dual SPI configuration. The configuration can be changed with R439, R440 and R441 (see Figure 3). Ensure that the hardware configuration used is matching to the software configuration of the S32K358.

Figure 3. SPI Configuration

Figure 3. SPI configuration

4. Install Software

4.1 Install Software

Download and install the following software: