Why Imaging Radar Matters for Advanced Driving
Driving automation introduces increasingly complex perception challenges. Vehicles must reliably detect vulnerable road users, distinguish closely spaced objects and operate consistently in dense traffic, poor weather or low‑visibility environments. Imaging radar rises to these challenges by providing accurate Doppler measurement, fine angular resolution and rich point‑cloud data. delivering consistent, high-fidelity perception regardless of environmental conditions.
A Scalable, Third‑Generation Radar Platform
NXP’s third‑generation imaging radar platform is designed to support a wide range of radar configurations while maintaining a scalable system architecture. By combining the S32R radar processing family with advanced radio frequency-complementary metal-oxide-semiconductor (RF-CMOS) radar transceiver technology, OEMs and Tier‑1 suppliers can scale performance efficiently across vehicle segments and regions.
S32R47 high-performance radar processor delivers the processing capability for robust object detection while maintaining a compact footprint and low power consumption
Unlocking High‑Performance Imaging Radar with Advanced RF Integration
A key building block of this platform is NXP’s latest RF-CMOS automotive radar transceiver— the TEF8388— integrating eight transmit and eight receive channels on a single monolithic die. The optimized RF architecture, pin assignment and launcher placement improve signal quality and reduce system bill of materials (BOM) with excellent power efficiency.
The TEF8388 radar transceiver integrates eight transmit and eight receive channels with full support for scaling from 8T8R to 32T32R configurations
From Technology to Series Production
High resolution imaging radar is rapidly transitioning from an emerging technology to broad real world deployment.
FORVIA HELLA is leveraging NXP’s advanced radar transceiver and processing technology as a key building block in its next generation radar sensor solutions . The first high resolution imaging radar program for a major car OEM—based on this third generation platform—is scheduled to enter series production in mid 2028.
This milestone demonstrates how the latest imaging radar technology innovation can deliver on demanding performance requirements while maintaining competitiveness for volume production at scale.
High-resolution radar sensors (“ForWave7HD”) for automated driving at SAE Level 2+ and beyond
Enabling the Next Wave of ADAS and Automated Driving
By bringing together high performance, enhanced power efficiency and a streamlined BOM, NXP’s third‑generation imaging radar platform helps accelerate the rollout of advanced perception platforms and supports the next wave of driving automation as vehicles evolve toward software‑defined architectures.
To learn more about NXP’s imaging radar portfolio, visit nxp.com/radar.
The project High Resolution Radar (HRR) L2+ to L4 ADAS and AD passenger vehicles based on NXP's 3rd generation imaging radar solution got awarded with the Tech.AD Award 2026