NXP Semiconductors in Chandler Celebrates 30 Years of Innovation
Processing thousands of wafers per week, Chandler Fab boosts the local economy and global availability of the most advanced automotive-grade semiconductors.
Sept 3, 2024
The SDV is designed to be enhanced over its lifetime through over-the-air updates. New cloud-based virtualization allows for development to take place before silicon is available and after the car is on the road.
Head of Vehicle System Engineering, NXP Semiconductors
Aug 5, 2024
Processing thousands of wafers per week, Chandler Fab boosts the local economy and global availability of the most advanced automotive-grade semiconductors.
Tags: We Are NXP
Nov 20, 2023
NXP and Advantest have collaborated with Arizona State University (ASU) to develop a pioneering engineering curriculum - The EEE 522 Radio Frequency Test.
Tags: We Are NXP
Oct 2, 2023
Mouser Electronics discusses its partnership with NXP for NXP Cup, the autonomous model vehicle competition coming in October 2024.
By Monica Tudora and Garance Aubert-Mazenq
Tags: We Are NXP
May 7, 2024
The mobile robotics industry is advancing rapidly thanks to technological improvements in sensors and electronics.
Apr 30 2024
OPC Unified Architecture (OPC UA) is a valuable tool for building interoperable Industry 4.0 systems and is compatible with MCX N974 and i.MX RT1180.
Tags: Factory Automation, Industrial
May 3, 2024
NXP can help automotive OEMs and Tier 1 suppliers achieve functional safety compliance in their automotive HMI designs with ready-to-deploy i.MX 95 applications processors
Sep 25, 2024
Learn about NXP's Software Defined Radio (SDR) platform—a tool revolutionizing affordable and accessible development hardware for industry and academia
By Harsha Master and Wim Rouwet
Tags: Connectivity, Industrial , Technologies
High performance and low power i.MX RT700 crossover MCUs for wearables, smart home, consumer, medical and HMI applications
By Eli Hughes
Tags: Smart Home
RW61x enables wireless connectivity for multiple implementations of the Matter standard such as Matter over: Thread, Wi-Fi and Ethernet.
Sep 20, 2024
The FRDM-RW612 and FRDM-MCXW71 boards allow developers to easily add Matter, Wi-Fi, Thread, Zigbee, or Bluetooth LE connectivity to smart home and industrial applications.
Tags: Industrial, Connectivity, Smart Home, Technologies,
Advances in microelectronics and software technologies are transforming auto infotainment and safety system design in big ways that are redefining the driving experience.
The SDV is designed to be enhanced over its entire lifetime. Along with completing software earlier in the development lifecycle, updates can also be delivered after vehicles are sold.
By Andy Birnie
Tags: Automotive, Vehicle Networking
Select i.MX and Layerscape® evaluation kits are now compatible with the newly released Debian 12 (based on the Linux kernel 6.6.3)
By Toby Foster
Tags: Technologies
Secure Element Management Services (SEMS) combats the widespread impact of the ROCA threat and the risks associated with eID card vulnerabilities
Tags: Identification , Smart City
Processing thousands of wafers per week, Chandler Fab boosts the local economy and global availability of the most advanced automotive-grade semiconductors.
Tags: We Are NXP
Join us as we dive deep into the issues behind today's connected world and explore our scalable solutions for our digitally-enhanced environment.
Subscribe to receive NXP Smarter World Blog articles and exclusive announcements.
GET THE NEWSLETTER