1
Out of the Box2
Get Software3
Build and Run4
Developer ExperienceSign in to save your progress. Don't have an account? Create one.

The following section describes the steps to boot the FRDM-IMX95-PRO board.
The kit contents include:
Get started developing your application on the FRDM-IMX95-PRO board with the out-of-the-box video. For more information, visit the i.MX 95 applications processor Documentation.
Something went wrong! Please try again.
The figure below shows the important components on the face of the FRDM-IMX95-PRO board.
The figure below shows the important components on the bottom of the FRDM-IMX95-PRO board.
Something went wrong! Please try again.
The FRDM-IMX95-PRO board comes with a pre-built NXP Linux binary demo image flashed on the eMMC. Without modifying the binary inside, booting from the eMMC provides a default system with certain features for building other applications on top of Linux.
To understand more about NXP’s Embedded Linux, continue reading the next sections.
Something went wrong! Please try again.
Connect the supplied USB Type-C cable to the debug UART port J22, then connect the other end of the cable to a host computer.
Four UART interfaces will be detected on the host computer. It is strongly recommended to open all four, since the port mapping for A55, M33 and M7 cores is not fixed.
If you are unfamiliar with terminal applications, view one of the following tutorials before continuing to step 1.5 Connect the HDMI display: Minicom Tutorial, Tera Term Tutorial, PuTTY Tutorial.
To debug under Linux, make sure that CH9114F Linux driver is installed.
Something went wrong! Please try again.
To experience the user interface provided with the image binary, Connect an HDMI cable to HDMI connector J21.
Something went wrong! Please try again.
SW4 [1-4] is the boot configuration switch. By default, the boot device is eMMC/uSDHC1.
BOOT_MODE3 SW4[1]
|
BOOT_MODE2 SW4[2]
|
BOOT_MODE1 SW4[3]
|
BOOT_MODE0 SW4[4]
|
Boot core | Boot device |
|---|---|---|---|---|---|
| x | 0 | 0 | 1 | Cortex-M33 | Serial downloader (USB) |
| x | 0 | 1 | 0 | uSDHC1 8-bit eMMC 5.1 | |
| x | 0 | 1 | 1 | uSDHC2 4-bit SD3.0 | |
| x | 1 | 0 | 0 | FlexSPI serial NOR Flash |
Something went wrong! Please try again.
Connect a USB PD charger to J11 using the USB Type-C to Type-C cable. Then power up the board by sliding the power switch SW1. The USB PD charger should support 20V/5A output.
The board has been set up to boot from eMMC by default. The processor starts executing the bootable image from eMMC. Then, the U-Boot execution should begin automatically.
Information is printed in the serial console for the Arm Cortex-A55. If you do not stop the U-Boot process, it continues to boot the kernel.
As the board boots up, you will see that penguins appear in the upper left-hand corner of the monitor, and then you will see the Linux terminal Icon on the top left and timer on right top corner. Congratulations, you are up and running.
Something went wrong! Please try again.
The i.MX Linux board support package (BSP) is a collection of binary files, source code and support files that are used to boot an Embedded Linux image on a specific i.MX development platform.
Current releases of Linux binary demo files can be found on Linux download page. Additional documentation is available in the i.MX Linux documentation bundle under the Linux sections of the i.MX Software and Development Tools.
FRDM-IMX95-PRO board supports booting from eMMC and SD card.
This Getting Started guide only outlines a few methods of transferring the Linux BSP to an SD card. To transfer to on-board eMMC, simply replace sd with emmc in all the commands. Experienced Linux developers can explore other options if desired.
Something went wrong! Please try again.
The latest pre-built images for the FRDM-IMX95-PRO board are available on the Linux download page under the most recent Linux version.
The pre-built NXP Linux binary demo image provides a typical system and basic set of features for using and evaluating the processor. Without modifying the system, the users can evaluate hardware interfaces, test SoC features and run user space applications.
Something went wrong! Please try again.
In addition to the connections from Section Out of the Box, connect the USB C (J7) to the host machine using the proper USB cable.
Unplug the power adapter. Consult the Section 1.6 Boot Switch Setup and configure the board to boot on serial download protocol (SDP) mode.
Depending on the OS used in the host machine, the way to transfer the Linux BSP image onto an SD card can vary. Choose an option below for detailed instructions:
Below are the instructions for Linux Host.
Download the latest stable files from UUU GitHub page . If further assistance for UUU is needed, please refer to this extensive tutorial .
uuulibusb1 (via apt-get or any other package manager)By default, this procedure flashes the image to the SD card. Check the UUU GitHub page for reference on how to flash the image to other devices.
Open a terminal application and change the directory to the location where uuu and the latest Linux distribution for FRDM-IMX95-PRO board are located. Add execution permission to the uuu file and execute it. uuu will wait for the USB device to connect.
$ chmod a+x uuu
$ sudo ./uuu -b sd_all imx-boot-imx95-19x19-lpddr5-frdm-pro-sd.bin-flash_a55 imx-image-full-imx95evk.wic.zstConfirm that FRDM-IMX95-PRO board boot mode is switched to serial download mode, and turn on the board, uuu will write the flash image to the board.
When it finishes, turn off the board. Consult the Section 1.6 Boot Switch Setup to configure the board to boot from an SD card. Power on the board to boot.
Below are the instructions for Windows Host.
Download the latest stable files from UUU GitHub page . If further assistance for UUU is needed, please refer to this extensive tutorial .
uuu.exeBy default, this procedure flashes the image to the SD card. Check the UUU GitHub page for reference on how to flash the image to other devices.
Open the command prompt application and navigate to the directory where the uuu.exe file and the Linux release for the FRDM-IMX95-PRO are located.
.\uuu.exe -b sd_all imx-boot-imx95-19x19-lpddr5-frdm-pro-sd.bin-flash_a55 imx-image-full-imx95evk.wic.zstConfirm that FRDM-IMX95-PRO board boot mode is switched to serial download mode, and turn on the board, uuu will start to flash the images to the board.
When it finishes, turn off the board. Consult the Section 1.6 Boot Switch Setup to configure the board to boot from an SD card. Power on the board to boot.
Something went wrong! Please try again.
In this section, a brief guide of how to build Yocto BSP image for FRDM-IMX95-PRO is introduced.
The FRDM-IMX95-PRO board BSP release is quarterly released with the i.MX family Linux BSP release. To build FRDM-IMX95-PRO image from source code, please first check i.MX Yocto Project User’s Guide to get familiar with Yocto project and Yocto build. Then please follow the steps below to build image for FRDM-IMX95-PRO. Here LF6.18.20 2.0.0 BSP is used as an example.
$ repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-wrynose -m imx-6.18.20-2.0.0.xml
$ repo sync$ MACHINE=imx95-19x19-lpddr5-frdm-pro DISTRO=fsl-imx-xwayland source imx-setup-release.sh -b frdm-imx95-pro$ bitbake imx-image-full$ zstdcat imx-image-full-imx95-19x19-lpddr5-frdm-pro.rootfs.wic.zst | sudo dd of=/dev/sdx bs=1M && syncOr using uuu to burn image into SD card:
$ uuu -b sd_all imx-image-full-imx95-19x19-lpddr5-frdm-pro.rootfs.wic.zstSW1[1:4] to “0011” to select SD card boot, insert the SD card and power up the FRDM-IMX95-PRO board.Something went wrong! Please try again.
To enable faster development for users of all skill levels, NXP provides extensive example applications to showcase various features and capabilities of the platform.
The Application Code Hub (ACH) repository enables engineers to easily find microcontroller and processor software examples, code snippets, application software packs and demos developed by NXP in-house experts. This space provides a quick, easy and consistent way to find microcontrollers and processor applications.
ACH provides filter and search options to quickly find specific applications. With the support of Git capabilities, there is an easy way to import and use applications within user’s development environments.
To learn more details of ACH, please visit this link.
To find available example applications for FRDM-IMX95, select i.MX in Device Families as shown below.
Select each example application to check for details.
To get the source code of each example application, click the Visit on GitHub button on the top to visit the code repository in NXP GitHub.
Something went wrong! Please try again.
The GoPoint for i.MX Application Processors is a user-friendly application launches pre-built applications packed with the Linux BSP, giving users an excellent out-of-the-box experience and hands-on experience with i.MX SoC's capabilities. GoPoint highlights advanced features while providing practical solutions for implementation, with source code and build recipes for the applications provided in GitHub .
To learn more details of GoPoint, please visit this link.
For FRDM-IMX95-PRO, GoPoint is included in the BSP release by default. To open the GoPoint GUI launcher, press the GoPoint logo displayed on the top left-hand corner of the screen after the FRDM-IMX95-PRO boot up as shown below.
Available example applications are shown with icons of screenshot for each application. When selecting the example application, a brief description of this example application is shown on the right side. To launch the currently selected application, click the Launch Demo button.
After an application is started, it can then be force-quit by clicking the Stop Current Demo button in the launcher (appears once the application is started).
For more details of the usage for each application, refer to GoPoint for i.MX Applications Processors User Guide (document GPNTUG).
Something went wrong! Please try again.
FRDM-IMX95-PRO uses CH9114F chip for the serial ports. The serial-to-USB drivers are available at CH342F Linux Drivers .
On the command prompt of the Linux host machine, run the following command to determine the port number:
$ ls /dev/ttyCH343USB*It should have 4 ports. Let’s say ttyCH343USB0-3.
It is strongly recommended to open all four, since the port mapping for Arm Cortex-A55, Arm Cortex-M33, and Arm Cortex-M7 core is not fixed.
Use the following commands to install and run the serial communication program (minicom as an example):
$ sudo apt-get install minicom$ sudo minicom /dev/ttyCH343USB* -sChoose Serial port setup and enter Configure Minicom as shown in the figure below.
After completing all the settings, press enter to go back to the above configuration window, then go to the Exit tab and press enter. Minicom will start to display message from the board serial port.
The CH9114F USB-serial chip on FRDM-IMX95-PRO enumerates 4 serial ports. Assume that the ports are COM11, COM12, COM13, COM14. The first Port (COM11) is for the serial console communication from Arm Cortex-M7. The third port (COM13) is for Arm Cortex-A55. The fourth port (COM14) is for System Manager running on Arm Cortex-M33.
Drivers will be installed automatically via Windows Update if connected to the internet. The serial-to-USB drivers are available at CH342F Windows Driver .
Note: To determine the port number of the i.MX board virtual COM port, open the Windows device manager and find USB serial Port in Ports (COM and LPT).
Tera Term is an open-source terminal emulation application. This program displays the information sent from the NXP development platform’s virtual serial port.
PuTTY is a popular terminal-emulation application. This program displays the information sent from the NXP development platform’s virtual serial port.
FRDM-IMX95-PRO has one general-purpose Arm Cortex-M7 running up to 800 MHz, which can be used for real-time and low-power processing. For how to build program and run program on Cortex-M7 core, developers can refer to application note AN14748 “How to Run Application on M7 Core of i.MX 95”.
For how to debug program running on Cortex-M7 core, developers can refer to application note AN14120 “Debugging Cortex-M with VS Code on i.MX 8M, i.MX 8ULP, and i.MX 9”.
Note: The Yocto build already includes several Cortex-M7 example images under rootfs /lib/firmware/ folder for quick evaluation and validation.
FRDM-IMX95-PRO has a Neural Processing Unit (NPU) operating at up to 8eTOPS to accelerate neural-network machine learning inference. For more details of the hardware architecture of NPU, please check i.MX 95 Applications Processor Reference Manual. For more details of software architecture of NPU, please check i.MX Machine Learning User's Guide.
To be accelerated by the NPU, the neural-network operators must be quantized to 8-bit unsigned or signed. For model quantization, please download latest eIQ toolkit and check the user guide.
To be accelerated by the NPU, the quantized model needs to be converted using the neutron-converter tool. The latest neutron-converter tool is included in the eIQ Neutron SDK, which can be downloaded from eIQ toolkit page. Please follow the user guide in the eIQ Neutron SDK to convert the model for i.MX95.
To evaluate NN model’s performance on NPU, the simplest method is to use the benchmark_model tool in Linux BSP. It uses random data as input and gives average inference time for a given number of runs. Here is an example:
root@imx95frdm:~# /usr/bin/tensorflow-lite-2.19.0/examples/benchmark_model --graph=/usr/bin/tensorflow-lite-2.19.0/examples/mobilenet_v1_1.0_224_quant_converted.tflite --external_delegate_path=/usr/lib/libneutron_delegate.soFor how to write code in c++ and python to run model inference on NPU, please refer to example applications in GoPoint .
FRDM-IMX95-PRO has one Arm Cortex-M33 running up to 333 MHz, which is dedicated to running a system manager (SM). SM is an application provided by NXP, intended to manage low-level resources for the other processors in the SoC.
The Cortex-M33 is the boot core, runs the boot ROM which loads the SM (and other boot code), and then branches to the SM. The SM then configures some aspects of the hardware such as isolation mechanisms and then starts other cores in the system. After starting these cores, it enters a service mode where it provides access to clocking, power, sensor, and pin control via a client RPC API based on ARM's System Control and Management Interface (SCMI) . To facilitate isolation between cores, the SM partitions the SoC into logical machines (LM) which have statically configurable access rights to both hardware and RPC API calls.
SM is delivered in source form in Github imx-sm repository, allowing customers the freedom to modify and recompile its code to suit their needs. However, NXP advises that any changes made to extend SM functionality must be limited to the customer board layer. To extend SM functionality, developers can refer to the Extending i.MX 9 System Manager Functionality with Board Controls (document AN14478).
FRDM-IMX95-PRO has a Video Processing Unit (VPU) including both decoder and encoder, which supports H.264, H.265 4Kp30 decoding, and H.264, H.265 4Kp30 encoding.
To test the VPU, the simplest way is to play an MP4 video file using following command:
root@imx95frdm:~# gplay-1.0 MP4_EXAMPLE_FILE.mp4The gplay-1.0 will automatically choose VPU as video decoder and play the MP4 file on the Weston desktop. You should be able to see the video playing on the HDMI display if connected.
For more details of how to use VPU API in applications, refer to the i.MX VPU Application Programming Interface Linux Reference Manual (document RM00294).
FRDM-IMX95-PRO has 500Mpixel/s MIPI_CSI and ISP (2x 4 lane, 2.5Gbps/lane) with PHY (1 mux with DSI) Camera interface, which supports up to 1x4Kp60fps, 2x4Kp30, 4x1080p60, or 8x1080p30 cameras with MIPI virtual channels.
To test the ISP, you can use EXPI-OS08A20 camera with FRDM-IMX95-PRO.
Note: Make sure OS08A20 camera is connected to the MIPI_CSI port of FRDM-IMX95-PRO before power up the board. Then please make sure you are using “imx95-19x19-frdm-pro-os08a20-isp.dtb” to boot the Linux OS.
u-boot=> setenv fdtfile imx95-19x19-frdm-pro-os08a20-isp.dtb
u-boot=> bootAfter FRDM-IMX95-PRO boots up with OS08A20 camera connected, please run following command to setup the environment and open camera preview of OS08A20:
root@imx95frdm:~# cam -l
root@imx95frdm:~# export LIBCAMERA_IPA_MODULE_PATH=/usr/lib/libcamera/ipa
root@imx95frdm:~# export LIBCAMERA_PIPELINES_MATCH_LIST='nxp/neo,uvc'
root@imx95frdm:~# export LIBCAMERA_IPA_CONFIG_PATH=/usr/share/libcamera/ipa
root@imx95frdm:~# export CAMERA0="/base/soc/bus@42000000/i2c@42540000/os08a20_mipi@36"
root@imx95frdm:~# gst-launch-1.0 libcamerasrc camera-name="${CAMERA0}" ! video/x-raw, width=3840, height=2160, format=YUY2 ! queue ! waylandsinkNote: "cam -l" command lists the available camera device paths. Update the CAMERA0 environment variable with the appropriate path reported by this command.
If camera preview is showed on the HDMI display with correct view, then it proves ISP is working fine.
For more details of ISP usage, refer the i.MX 95 Camera Porting Guide (document UG10215).
FRDM-IMX95-PRO has a Mali-G310 Graphics Processing Unit (GPU) operating at up to 60 GFLOPS (high-precision), which supports OpenGL ES 3.2, OpenCL 3.0, Vulkan 1.2.
To test the GPU performance, the simplest way is to run glmark2-es2-wayland benchmark as following command:
root@imx95frdm:~# glmark2-es2-wayland --fullscreenBesides this, there are many other GPU example applications installed in the FRDM-IMX95-PRO default rootfs under folder /opt/imx-gpu-sdk/, you can try them by directly executing the binary or launch the application from GoPoint.
For more details of GPU usage, refer to the i.MX Graphics User's Guide (document UG10159).
In certain use cases, there is requirement for the minimum device boot time, which means the device needs to complete booting in a given time limit.
To optimize the boot time, FRDM-IMX95-PRO supports falcon mode in U-Boot. Falcon mode is a feature in U-Boot that enables fast booting by allowing SPL to directly start the Linux kernel. It completely skips the U-Boot loading and initialization, with the effect of reducing the time spent in the bootloader.
For how to enable falcon mode and further optimize boot time, refer to the Fast Boot on i.MX 8 and i.MX 9 Using Falcon Mode and Kernel Optimizations (document AN14093).
Kit Contents/Packing List
Get Familiar with the Board
Boot from eMMC
Connect USB Debug Cable
Connect the HDMI Display
Boot Switch Setup
Connect Power Supply