1
Out of the Box2
Get Hardware3
Plug It In4
Build, LoadSign in to save your progress. Don't have an account? Create one.

The KITPF9455FRDMPGM board kit allows you to evaluate, design, implement and validate the PF9455 power management-integrated circuit (PMIC) for high-performance applications.
This getting started guide will walk you through the process of setting up and using the KITPF9455FRDMPGM board.
The kit contents include:
Something went wrong! Please try again.
In addition to the kit contents, the following hardware provides further support when using this board.
Something went wrong! Please try again.
You will need a Windows PC workstation to evaluate the board. For best results, please use the following equipment:
Something went wrong! Please try again.
Before working with the board, you will need to install software. You can find the software at the PF9455 evaluation board's page or from the NXP PMIC Graphical User Interface (GUI).
Something went wrong! Please try again.
The KITPF9455FRDMPGM evaluation board includes the following features:
Something went wrong! Please try again.
The KITPF9455FRDMPGM evaluation board integrates a KL25Z MCU to support communication between the board and the PC-based GUI to control and monitor of the PF9455 device.
Something went wrong! Please try again.
The diagram below shows you the communication paths between the components.
Figure 2 below shows the placement of connectors, configuration headers and LED indicators on the KITPF9455FRDME evaluation board. For information on the default jumper and switch configuration, refer to the KITPF9455PGM product page.
Something went wrong! Please try again.
Follow the steps below to set up the KITPF9455FRDMPGM board:
To launch the PF9455 NXP GUI:
Something went wrong! Please try again.
This section will walk you through the KITPF9455FRDMPGM program board. It covers the features associated with each jumper and switch, details on enabling features through hardware configuration and advice on the LED signaling and test points available on the board.
Note: The board silkscreen provides jumper-position guidance based on the selected function. The default debug configuration enables the board to be fully controlled by the KL25Z MCU (via I²C) and the GUI. Figure 2 shows the default jumper and switch configuration for the PF9455.
Table 1. Configuration Jumpers.
| Connector | Pin count | Line | Connection |
|---|---|---|---|
J1/J2/J3/J4 |
--- | FRDM board headers | --- |
J17 |
1 | SW2OUT | Open |
| 2 | SW3OUT | Open | |
J18 |
1 | SW4OUT | Open |
| 2 | SW5OUT | Open | |
J29 |
1 | Pullup for RSTB | Jumper connected |
| 2 | RSTB | ||
J23 |
1 | VIN | Open |
| 2 | GND | Open | |
J24 |
1 | VIN | Open |
| 2 | USB_PWR | ||
| 3 | VIN | Open | |
| 4 | 3V3_MCU | ||
J25 |
1 | VDDIO | Jumper connected |
| 2 | 3V3_MCU | ||
J26 |
1 | VIN | Open |
| 2 | PWRON | Open | |
| 3 | GND | Open | |
J27 |
1 | SCL | Open |
| 2 | PWRON | Open | |
| 3 | SDA | Open | |
| 4 | VDDOTP | Open | |
| 5 | IO1 | Open | |
| 6 | VDDIO | Open | |
| 7 | R127 0 ohm to VIN | Open | |
| 8 | GND | Open | |
| 9 | Open | Open | |
| 10 | Open | Open |
Table 2. Access Point Functions.
| Function | Description | Color |
|---|---|---|
| Low-dropout regulator 1 input (LDO1IN) | Monitoring point for the low-dropout regulator 1 (LDO1) input voltage | Red |
| Low-dropout regulator 2 input (LDO2IN) | Monitoring point for the low-dropout regulator 2 (LDO2) input voltage | Red |
| Low-dropout regulator 3 input (LDO3IN) | Monitoring point for the low-dropout regulator 3 (LDO3) input voltage | Red |
| VSWIN | Switchers input voltage | Red |
| Power supply (VIN) | External Input voltage | Red |
| Low-dropout regulator 1 output voltage (VLDO1) | Monitoring point for the LDO1 output | White |
| Low-dropout regulator 2 output voltage (VLDO2) | Monitoring point for the LDO2 output | White |
| Low-dropout regulator 3 output voltage (VLDO3) | Monitoring point for the LDO3 output | White |
| Ground (GND) | Board grounds direct connection -4 easy access points | White |
| Always-on voltage output (VAON) | Monitoring point for the VAON output | White |
| Switcher 1 (SW1) output | Monitoring point for the SW1 output | White |
| Switcher 2 (SW2) output | Monitoring point for the SW2 output | White |
| Switcher 3 (SW3) output | Monitoring point for the SW3 output | White |
| Switcher 4 (SW4) output | Monitoring point for the SW4 output | White |
| Switcher 5 (SW5) output | Monitoring point for the SW5 output | White |
| General-purpose input/output 1 (GPIO1) | GPIO1 access point, bidirectional pin | White |
| General-purpose input/output 2 (GPIO2) | GPIO2 access point, bidirectional pin | White |
| General-purpose input/output 3 (GPIO3) | GPIO3 access point, bidirectional pin | White |
| General-purpose input/output 4 (GPIO4) | GPIO4 access point, bidirectional pin | White |
| Voltage monitor 1 (VMON1) | Monitoring point for the external monitor VMON1 | White |
| Voltage monitor 2 (VMON2) | Monitoring point for the external monitor VMON2 | White |
| Digital voltage output (VDIG) | VDIG monitoring point | White |
| Analog voltage output (VANA) | VANA monitoring point | White |
| Power on input (PWRON) | Power on input pin access point | White |
| Input/output supply voltage (VDDIO) | VDDIO Monitoring point | White |
| Reset signal output (RSTB) | System reset signal output monitoring point | White |
| One-time programmable supply voltage (VDDOTP) | VDDOTP Monitoring point | White |
| Interintegrated circuit-serial data access point | I²C SDA, bidirectional pin | White |
| Interintegrated circuit-serial clock access point | I²C SCL, bidirectional pin | White |
Note: Test points are routed directly to the pins.
Something went wrong! Please try again.