1
Plug It In2
Get Software3
Install and ImportSign in to save your progress. Don't have an account? Create one.
Take FRDM-K64F as an example for demo.
Something went wrong! Please try again.
Connect the board to the PC via the USB cable between the OpenSDA USB port on the board and the USB connector on the PC.
Something went wrong! Please try again.
Kinetis MCU boards are supplied with OpenSDA firmware pre-loaded. For software development on the MCU board, make sure the latest OpenSDA driver is on the FRDM development board. This allows debugging, flash programming and serial communication over a USB cable. Find the latest OpenSDA firmware for the boards here:
OpenSDA Update to the boardsFor the example, FRDM-K64F, go to this website and choose board FRDM-K64F to get the latest OpenSDA firmware.
Something went wrong! Please try again.
The output data from the provided example applications are provided over the MCU UART. This requires that the driver for the board’s virtual COM port is installed. The board MUST be plugged into the PC before the driver installer is run.
The links for the latest OpenSDA Windows serial port drivers are provided on the same web:
OpenSDA Update to the boardsFor the example, FRDM-K64F, go to this website and choose board FRDM-K64F. In the coming webpage, click on Arm CMSIS-DAP serial drivers to download Windows Serial Port Drivers.
Once the Windows Serial Port Drivers are installed on the PC, determine the port number of the FRDM board’s virtual COM port by opening the device manager and looking under the "Ports" group.
Note: All the Serial Port Drivers are included and installed automatically when installing MCUXpresso IDE. Skip this step and jump to section 2 if MCUXpresso IDE is planned to install.
The demonstration board is now ready to communicate with the PC.
Something went wrong! Please try again.
Something went wrong! Please try again.
Click on Download SDK. A pop-up window SDK Download will show when the package is built successfully. Click on Download SDK Archive to download the package. The package is provided as a zip file.
Something went wrong! Please try again.
NXP offers a complimentary toolchain called MCUXpresso IDE.
Get MCUXpresso IDE
No problem! The MCUXpresso SDK includes support for other tools such as IAR, Keil.
Something went wrong! Please try again.
Install the downloaded FRDM-K64F SDK package into MCUXpresso IDE (Simply drag and drop the zipped SDK package as it is to the “Installed SDKs” view).
Once the SDK installation is completed, click on ‘Import SDK examples’.
Import freedom_bootloader example from the list of available projects.
Note: Once, the freedom_bootloader example is imported successfully, the MCUXpresso IDE automatically creates the corresponding standalone project in your workspace.
Something went wrong! Please try again.
Build the project by clicking 'build' button.
Load firmware by clicking on “Debug frdmk64fxx”
Something went wrong! Please try again.
Before running blhost, get the port number of the FRDM board’s virtual COM port by opening the device manager and looking under the "Ports" group.
In downloaded package, Windows blhost is located at
middleware\mcu-boot\bin\Tools\blhost\win.
Open a command prompt and run blhost to initiate communication and inject commands to the bootloader. For instance, you can connect to bootloader over UART with an option "-p" and run blhost command get-property to get some information from bootloader.
Type blhost -p COM21 -- get-property 12 to get memory regions reserved by the Bootloader.
Type blhost -p COM21 -- get-property 1 to get current bootloader version.
For more details, please refer to blhost User’s Guide.
Tera Term is a very popular open source terminal emulation application. This program can be used to display information sent from your NXP development platform's virtual serial port.
PuTTY is a popular terminal emulation application. This program can be used to display information sent from your NXP development platform's virtual serial port.
No problem! Your board simply came in the old packaging and has a different out-of-box demo loaded into the flash memory.
You should be seeing the RGB LED toggling between each of the three colors; red, blue and green. It's OK to move onto the next step when you're ready.
Try proceeding to the next steps to get other example applications running on your board. If you still have problems, try contacting us through the NXP Community.
The following steps will guide you through opening the hello_world application. These steps may change slightly for other example applications as some of these applications may have additional layers of folders in their path.
If not already done, open the desired example application workspace. Most example application workspace files can be located using the following path:
<install_dir>/boards/<sdk_board_name>/<example_type>/<application_name>/iar
Using the hello_world demo as an example, the path is:
<install_dir>/boards/frdmk64f/demo_apps/hello_world/iar
Select the desired build target from the drop-down. For this example, select the “hello_world – Debug” target.
To build the application, click the “Make” button, highlighted in red below.
The build will complete without errors:
The FRDM-K64F board comes loaded with the mbed/CMSIS-DAP debug interface from the factory. If you have changed the debug OpenSDA application on your board, visit http://www.nxp.com/opensda for information on updating or restoring your board to the factory state.
Connect the development platform to your PC via USB cable between the "SDAUSB" USB port on the board and the PC USB connector.
Open the terminal application on the PC (such as PuTTY or TeraTerm) and connect to the debug COM port you determined earlier. Configure the terminal with these settings:
Click the "Download and Debug" button to download the application to the target.
The application is then downloaded to the target and automatically runs to the main() function.
Run the code by clicking the "Go" button to start the application.
The hello_world application is now running and a banner is displayed on the terminal. If this is not the case, check your terminal settings and connections.
After the MDK tools are installed, Cortex® Microcontroller Software Interface Standard (CMSIS) device packs must be installed to fully support the device from a debug perspective. These packs include things such as memory map information, register definitions and flash programming algorithms. Follow these steps to install the appropriate CMSIS pack.
Open the MDK IDE, which is called µVision. In the IDE, select the "Pack Installer" icon.
In the Pack Installer window, navigate to the section with the Kinetis packs (they are in alphabetical order). The Kinetis packs start with "Keil::Kinetis" and are followed by the MCU family name, for example, "Keil::Kinetis_K60_DFP". Because this example uses the FRDM-K64F platform, the K60 family pack is selected. Click on the "Install" button next to the pack. This process requires an Internet connection to successfully complete.
After the installation finishes, close the Pack Installer window and return to the µVision IDE.
The following steps will guide you through opening the hello_world application. These steps may change slightly for other example applications as some of these applications may have additional layers of folders in their path.
If not already done, open the desired demo application workspace in:
<install_dir>/boards/<sdk_board_name>/<example_type>/<application_name>/mdk
The workspace file is named <application_name>.uvmpw, so for this specific example, the actual path is:
<install_dir>/boards/frdmk64f/demo_apps/hello_world/mdk/hello_world.uvmpw
To build the demo project, select the "Rebuild" button, highlighted in red.
The build will complete without errors.
The FRDM-K64F board comes loaded with the mbed/CMSIS-DAP debug interface from the factory. If you have changed the debug OpenSDA application on your board, visit http://www.nxp.com/opensda for information on updating or restoring your board to the factory state.
Connect the development platform to your PC via USB cable between the "SDAUSB" USB port on the board and the PC USB connector.
Open the terminal application on the PC (such as PuTTY or TeraTerm) and connect to the debug COM port you determined earlier. Configure the terminal with these settings:
After the application is properly built, click the "Download" button to download the application to the target.
After clicking the "Download" button, the application downloads to the target and should be running. To debug the application, click the "Start/Stop Debug Session" button, highlighted in red.
Run the code by clicking the "Run" button to start the application.
The hello_world application is now running and a banner is displayed on the terminal. If this is not the case, check your terminal settings and connections.
The following steps will guide you through opening the hello_world example.
Find the Quickstart Panel in the lower left hand corner
Then click on Import SDK examples(s)…
Click on the frdmk64f board to select that you want to import an example that can run on that board, and then click on Next.
Use the arrow button to expand the demo_apps category, and then click the checkbox next to hello_world to select that project. To use the UART for printing (instead of the default semihosting), clear the “Enable semihost” checkbox under the project options. Then, click on Next.
On the Advanced Settings wizard, clear the checkbox “Redirect SDK “PRINTF” to C library “printf”“ in order to use the MCUXpresso SDK console functions for printing instead of generic C library ones. Then click on Finish.
Now build the project by clicking on the project name and then click on the Build icon.
You can see the status of the build in the Console tab.
MCUXpresso IDE will probe for connected boards and should find the MBED CMSIS-DAP debug probe that is part of the integrated OpenSDA circuit on the FRDM-K64F. Click on OK to continue.
The firmware will be downloaded to the board and the debugger started.
Open up a terminal program and connect to the COM port the board enumerated as. Use 115200 baud 8 data bits, no parity and 1 stop bit.
Start the application by clicking the "Resume" button:
The hello_world application is now running and a banner is displayed on the terminal. If this is not the case, check your terminal settings and connections.
Use the controls in the menu bar to pause, step into, and step over instructions and then stop the debugging session by click on the Terminate icon:
This section contains the steps to install the necessary components required to build and run a KSDK demo application with the Arm GCC toolchain, as supported by the Kinetis SDK. There are many ways to use Arm GCC tools, but this example focuses on a Windows environment. Though not discussed here, GCC tools can also be used with both Linux OS and Mac OSX.
Download and run the installer from launchpad.net/gcc-arm-embedded. This is the actual toolchain (i.e., compiler, linker, etc.). The GCC toolchain should correspond to the latest supported version, as described in the Kinetis SDK Release Notes.
The Minimalist GNU for Windows (MinGW) development tools provide a set of tools that are not dependent on third-party C-Runtime DLLs (such as Cygwin). The build environment used by the KSDK does not use the MinGW build tools, but does leverage the base install of both MinGW and MSYS. MSYS provides a basic shell with a Unix-like interface and tools.
Download the latest MinGW mingw-get-setup installer from sourceforge.net/projects/mingw/files/Installer/.
Run the installer. The recommended installation path is C:\MinGW, however, you may install to any location.
NOTE
The installation path cannot contain any spaces.
Ensure that the "mingw32-base" and "msys-base" are selected under Basic Setup.
Click "Apply Changes" in the "Installation" menu and follow the remaining instructions to complete the installation.
Add the appropriate item to the Windows operating system Path environment variable. It can be found under Control Panel -> System and Security -> System -> Advanced System Settings in the "Environment Variables..." section. The path is:
<mingw_install_dir>\bin
Assuming the default installation path, C:\MinGW, an example is shown below. If the path is not set correctly, the toolchain does not work.
NOTE
If you have "C:\MinGW\msys\x.x\bin" in your PATH variable (as required by KSDK 1.0.0), remove it to ensure that the new GCC build system works correctly.
Create a new system environment variable and name it ARMGCC_DIR. The value of this variable should point to the Arm GCC Embedded tool chain installation path, which, for this example, is:
C:\Program Files (x86)\GNU Tools Arm Embedded\4.9 2015q3
Reference the installation folder of the GNU Arm GCC Embedded tools for the exact pathname of your installation.
Download CMake 3.0.x from www.cmake.org/cmake/resources/software.html.
Install CMake, ensuring that the option "Add CMake to system PATH" is selected when installing. It's up to the user to select whether it's installed into the PATH for all users or just the current user. In this example, the assumption is that it's installed for all users.
Follow the remaining instructions of the installer.
You may need to reboot your system for the PATH changes to take effect.
To build an example application, follow these steps.
1. If not already running, open a GCC Arm Embedded tool chain command window. To launch the window, from the Windows operating system Start menu, go to “Programs -> GNU Tools Arm Embedded <version>” and select “GCC Command Prompt”.
Change the directory to the example application project directory, which has a path like this:
<install_dir>/boards/<board_name>/<example_type>/<application_name>/armgcc
For this guide, the exact path is:
<install_dir>/boards/frdmk64f/demo_apps/hello_world/armgcc
Type “build_debug.bat” on the command line or double click on the "build_debug.bat" file in Windows operating system Explorer to perform the build. The output is shown in this figure:
The GCC tools require a J-Link debug interface. To update the OpenSDA firmware on your board to the latest J-Link app, visit www.nxp.com/opensda. After installing the J-Link OpenSDA application, download the J-Link driver and software package from www.segger.com/downloads.html.
Connect the development platform to your PC via USB cable between the "SDAUSB" USB port on the board and the PC USB connector.
Open the terminal application on the PC (such as PuTTY or TeraTerm) and connect to the debug COM port you determined earlier. Configure the terminal with these settings:
Open the J-Link GDB Server application. Assuming the J-Link software is installed, the application can be launched by going to the Windows operating system Start menu and selecting "Programs -> SEGGER -> J-Link <version> J-Link GDB Server".
Modify the settings as shown below. The target device selection chosen for this example is the “MK64FN1M0xxx12” and use the SWD interface.
After it is connected, the screen should resemble this figure:
If not already running, open a GCC Arm Embedded tool chain command window. To launch the window, from the Windows operating system Start menu, go to "Programs -> GNU Tools Arm Embedded <version>" and select "GCC Command Prompt".
Change to the directory that contains the demo application output. The output can be found in using one of these paths, depending on the build target selected:
<install_dir>/boards/<board_name>/<example_type>/<application_name>/armgcc/debug
<install_dir>/boards/<board_name>/<example_type>/<application_name>/armgcc/release
For this guide, the path is:
<install_dir>/boards/frdmk64f/demo_apps/hello_world/armgcc/debug
Run the command "arm-none-eabi-gdb.exe <demo_name>.elf". For this example, it is "arm-none-eabi-gdb.exe hello_world.elf".
Run these commands:
The application is now downloaded and halted at the reset vector. Execute the "monitor go" command to start the example application.
The hello_world application is now running and a banner is displayed in the terminal window.
Now export the pin_mux.c and pin_mux.h files by clicking on the Sources tab on the right side to get to the Sources view, and selecting the export icon.

Select the directory to export the pin_mux.c and pin_mux.h files. In this example export to the “board” folder in the led_output project in the workspace that was created in the previous section.
(i.e. C:\MCUXpressoIDE_Lab\frdmk64f_driver_examples_gpio_led_output\board). Select Finish.
Select the directory to export the clock_config.c and clock_config.h files. In this example export to the “board” folder in the led_output project in the workspace.
(i.e. C:\MCUXpressoIDE_Lab\frdmk64f_driver_examples_gpio_led_output\board). Select Finish.
Something went wrong! Please try again.