Getting Started with the KIT6X02AS2T1

Last Modified: May 26, 2026Supports Evaluation Board for BMA6X02 with SPI

Contents of this document

  • 1

    Out of the Box
  • 2

    Get Hardware
  • 3

    Configure Hardware

1. Out of the Box

The NXP analog product development boards provide an easy-to-use platform for evaluating NXP products. The boards support a range of analog, mixed-signal and power solutions. They incorporate monolithic integrated circuits (ICs) and system-in-package (SiP) devices that use proven high-volume technology. NXP products offer longer battery life, a smaller form factor, reduced component counts, lower cost and improved performance in powering state-of-the-art systems.

This page guides you through the process of setting up and using the KIT6X02AS2T1 board.

1.1 Kit Contents and Packing List

The KIT6X02AS2T1 includes:

  • KIT6X02AS2T1: SPI2TPL evaluation board for BMA6X02 with serial peripheral interface (SPI) and transport
  • Protocol link (TPL) communication
  • Cable for supply
  • Electrical transport protocol link (ETPL) cable, which is a two-wire twisted pair TPL cable (50 cm)

2. Get Hardware

The purpose of the KIT6X02AS2T1 is to allow a communication of a standard microcontroller (MCU) with NXP analog front-end (AFE) boards (for example, EVBMA7X18DT1 or EVBMA777T3).

2.1 Board Features

The main features of the KIT6X02AS2T1 are:

  • Communication link from SPI to TPL and back
  • Configuration options for the different SPI modes offered by the BMX6X02AS
  • Configuration options for the different clock modes offered by the BMX6X02AS
  • Configuration options for different supply concepts
  • Easy access to the serial peripheral interface (SPI) communication lines
  • Two galvanically isolated ETPL ports
  • Support for the transformer physical layer 3 (TPL3) protocol version
  • Three status LEDs

2.2 Board Description

The KIT6X02AS2T1 is an evaluation board designed for the BMX6X02 general-purpose battery management system (BMS) communication gateway and electrochemical impedance spectroscopy (EIS) synchronization controller (see Figure 1). It is equipped with a BMA6402AS device, which integrates the synchronization functionality required for EIS measurements. The BMA6402AS combines the full feature sets of the BMA6002AS, BMI6402AS and BMI6002AS, enabling the KIT6X02AS2T1 board to function as a versatile evaluation platform for all associated device variants.

2.3 Board Components

Figure 1. KIT6X02AS2T1 Overview

Figure 1. KIT6X02AS2T1 Overview

3. Configure Hardware

The KIT6X02AS2T1 has several configuration options. The most important ones are the clock and supply configuration (see Section 3.2) and the MCU interface (see Section 3.1).

3.1 MCU Interface

The MCU interface (see Figure 2) of the KIT6X02AS2T1 allows the connection toward the MCU.

Figure 2. KIT6X02AS2T1 MCU Interface

Figure 2. KIT6X02AS2T1 MCU Interface

All relevant pins of the BMX6X02 are routed to the MCU interface, enabling flexible and application-specific MCU connections, such as single SPI or dual SPI configurations. Because SPI signals typically operate at high frequencies, each SPI line is paired with an adjacent ground (GND) pin to ensure signal integrity and minimize noise. The connector pin assignments are listed in Table 1. With the board dual and single SPI operation can be achieved. For single SPI configuration, the SPI clock and the chip select pins must be connected. This connection can be achieved by an appropriate external wiring or by population of R15 and R16.

Pin number Function Description
1VSSground as reference
2CSN_RSP1. Target response SPI chip select input
2. Controller response SPI chip select output
3VSSground as reference
4SCLK_RSP1. Target response SPI clock input
2. Controller response SPI clock output
5VSSground as reference
6SDAT_RSP_TXDresponse SPI data output
7VSSground as reference
8CSN_REQrequest SPI chip select input
9VSSground as reference
10SCLK_REQrequest SPI clock input
11VSSground as reference
12SDAT_REQ_RXDrequest SPI data input
13VSSground as reference
14OSCPexternal clock positive input
15GPIO01. General-purpose input 0
2. General-purpose output 0
3. Interrupt 0 output (INT0)
16VSSground as reference
17GPIO11. General-purpose input 1
2. General-purpose output 1
3. Interrupt 1 output (INT1)
4. CSN3 for peripheral SPI controller
18STB_N_OUTstandby output, active LOW
19GPIO21. General-purpose input 2
2. General-purpose output 2
3. Interrupt 2 output (INT2)
4. CSN2 for peripheral SPI controller
20STB_OUTstandby output, active HIGH
21GPIO31. General-purpose input 3
2. General-purpose output 3
3. Interrupt 3 output (INT3)
4. CSN1 for peripheral SPI controller
22TPL_WAKEwake output of the evaluation board (EVB) for waking up of the system
23GPIO41. General-purpose input 4
2. General-purpose output 4
3. I²C bus SCL
4. SCLK for peripheral SPI controller
24RESETreset input of BMX6X02
25GPIO51. General-purpose input 5
2. General-purpose output 5
3. I²C bus SDA
4. Controller output target input (COTI) for peripheral SPI controller
26VSSground as reference
27GPIO61. General-purpose input 6
2. General-purpose output 6
3. Synchronization input
4. CSN0 for peripheral SPI controller
28VEXTexternal supply voltage for VDDIO
29GPIO71. General-purpose input 7
2. General-purpose output 7
3. Hold input
4. Controller input target output (CITO) for peripheral SPI controller
30VSSground as reference

3.2 Jumpers

The KIT6X02AS2T1 has three jumpers for the supply and clock selection (see Figure 3).

Figure 3. KIT6X02AS2T1 Jumpers

Figure 3. KIT6X02AS2T1 Jumpers

The supply jumpers can be used to realize different supply and clock concepts.

3.3 Supply Options

J3 (marked red) is used to select the voltage digital drain input/output (VDDIO) supply voltage.

  • When the jumper is placed in position 1-2, the VDDIO voltage is sourced from voltage regulator (VREG), the internal 5 V regulator of the BMX6X02S
  • When the jumper is placed in position 2-3, the VDDIO voltage is sourced from voltage external (VEXT). An external VEXT supply can be provided through connector J7, pin 29

J9 (marked blue) is used to select the voltage digital core (VDDC) voltage for the BMX6X02S

  • When the jumper is placed in position 1-2, the VDDC voltage is is sourced from VREG, the internal 5 V regulator of the BMX6X02S
  • Alternative 5 V sources can be directly applied to J9, pin 2

3.4 Clock Options

The BMX6X02S supports multiple clock source configurations (marked orange). By default, the device uses the external oscillator mounted on the KIT6X02AS2T1, providing a robust and stable reference suitable for EIS measurements.

To reduce system cost, the MCU may alternatively provide the clock signal through one of its general-purpose input/output (GPIO) pins. Because this signal operates at a high frequency, maintaining good signal integrity can be challenging. If the clock line is shielded and kept shorter than 10 cm, acceptable performance can still be achieved. For this configuration, inject the clock signal into J9, pin 14, remove the 0 Ω resistors at R17 and R22 and install one of them at R23, leaving R3 unpopulated. If EIS functionality is not required, the BMX6X02S can operate using its internal clock source. To enable the internal clock, place jumper J1 in position 2-3.