ACL Digital |
CENTAURI 200 IoT Gateway Platform |
NXP i.MX 6UL/6ULL, NXP KW41Z, NXP JN5169/JN5179, NXP A7101CHTK2 |
Arcane Four Software |
Ottawa Infotainment Dragon Fire Domain Controller Unit |
i.MX 8M Plus |
Arkamys |
SoundStage Mainstream |
NXP Quantum Q4 |
Arkamys |
SoundStage Digital Premium |
i.MX 8 |
Arkamys |
SoundStage Premium |
i.MX 8 |
Arkamys |
SoundStage Digital Premium HW |
i.MX 8 |
BARROT |
Automotive grade Bluetooth+Wi-Fi6 module i1890-sp (based on AW690) |
AW690 |
BARROT |
Automotive grade Bluetooth module i1647e-s |
KW47 |
BARROT |
Automotive grade Bluetooth+Wi-Fi6 module i1811-s |
AW611 |
BARROT |
Automotive grade Bluetooth+Wi-Fi6 module i1598-sp |
88Q9098 |
BARROT |
Bluetooth LE Audio demostration embedded with NXP chipset, and Bluetooth+Wi-Fi Automotive modules embedded with AW690, 693, 88Q9098 and Bluetooth modules embedded with KW38 |
AW690, AW693, 88Q9098, KW38 |
Digi International |
Digi ConnectCore 91 Wireless Edge to Cloud Connectivity |
i.MX 91, i.MX 93, IW611, PCA9451 |
Ecotron |
EV2274A |
SPC5744P |
Ecotron |
EV62314A |
S32K314 |
Elektrobit Automotive GmbH |
EB corbos Linux for Safety Applications |
S32G3, GoldBox 3 |
Elektrobit Automotive GmbH |
EB corbos Linux for Safety Applications on S32G |
S32G3 |
First International Computer, Inc. |
Automotive Augmented Reality Head-Up Display (ARHUD) Unit |
FS32K118 and series |
Fraunhofer IIS - upHear |
upHear Flexible Rendering - Automatic adaption of the immersive rendering to the current playback situation by intelligently handling arbitrary number of audio playback devices of potentially different size at arbitrary positions |
i.MX 8, SR250, NXH3675 |
Gateworks |
Wi-Fi 6 Development Kit |
IW611, i.MX 8M Mini |
Gateworks |
Venice Flex SBC |
i.MX 8M Plus |
Green Hills Software LLC |
CoreRide Gateway |
S32G3 |
Green Hills Software LLC |
CoreRide Zonal Controller |
S32E |
KAGA FEI CO., LTD. |
WKR612AA1, MCU embedded wireless combo module supporting Wireless LAN IEEE802.11a/b/g/n/ac/ax, Bluetooth® low energy and IEEE802.15.4 with built-in antenna and radio certification for Japan, FCC and ISED. |
RW612 |
KAGA FEI CO., LTD. |
WKI611AA1, Wi-Fi 6 and Bluetooth-supported wireless LAN/Bluetooth combo module with built-in antenna and radio certification for Japan, FCC and ISED. |
IW611 |
Kinara, Inc. |
Large Language and Vision Assistant Model |
i.MX 95 |
Kinara, Inc. |
Vehicle tracking |
i.MX 8M Plus |
Kinara, Inc. |
LLaMa2-7B with automatic speech recognition and text-to-speech |
i.MX 95 |
KPIT Technologies |
Integrated Vehicle Motion Control |
NXP S32G hardware |
KPIT Technologies |
Autonomous Driving Domain HIL |
S32G hardware |
KPIT Technologies |
Zonal Architecture Validation |
S32G hardware |
LINXENS |
Fox tracker. A smart label for logistic based on Flex technology. The label is also onboarding Temperature, Shocks and Accelerometer sensors. All the system can be activated by NFC. The energy is powered by a printed battery. |
- |
Leopard Imaging |
Leopard Imaging GS500 Smart City Vision System powered by Sony IMX500 AI sensor |
NXP i.MX 8M |
MicroEJ |
VEE Energy |
FRDM-MCXN947, MCXN947 |
MicroEJ |
Connected Thermostat |
FRDM-RW612, RW612 |
MicroEJ |
Washing Machine |
FRDM-IMX93, i.MX93, EVK i.MX93 |
P3 |
SPARQ OS-Android Automotive OS 14 turnkey infotainment (HMI) |
i.MX 95 |
P3 |
SPARQ OS - Android Automotive OS 14 turnkey infotainment (Cluster) |
i.MX 95 |
Qt Group |
SmartBooth Squish Lightbulb Demo; a smarthome demo that actually controls a light. |
i.MX 95 |
Qt Group |
Accelerate demo; coffee machine. |
i.MX 95, i.MX RT1050 |
Quectel |
IW612, IW611 and RW610 module. |
IW612, IW611, RW610 module |
Real-Time Innovations (RTI) |
Adaptive Headlamp System; this demonstrates the power of Connext Drive as it streamlines automotive development from simulation to production using off-the-shelf commercial software and hardware. |
S32G3 SoC, GoldBox 3 |
Real-Time Innovations (RTI) |
RTI will feature an adaptive headlamp system running on Connext Drive and NXP S32G3 to showcase end-to-end solutions from simulation to production. NXP will be featured in the Prototyping and Production areas, where we illustrate how to quickly create new concepts with off-the-shelf hardware, reusing the same code created for production; and then use the same software to move from early stage development to fleet using NXP automotive-grade hardware without custom coding. |
S32G3 |
RT-RKvRT-RK Computer Based Systems LLC |
mARTini Android Container Solution for Empowering Android Applications Within Linux Infotainment Hosts |
i.MX 8 Family – Arm® Cortex®-A53, Cortex-A72 |
s.m.s, smart microwave sensors GmbH |
DRVEGRD 166 is a 4D Imaging Radar with a much higher resolution compared to previous generations. Thanks to its special 3D Waveguide antenna and the high target separation capabilities, the sensor can process a lot more targets, delivering a very dense point cloud of up to 20.480 points per second. |
S32R45, 4 x NXP TEF8232 |
Sonatus |
Zonal Vehicle Network Manager |
S32G |
StreamUnlimited Engineering GmbH |
Reference Soundbar with Flexible Rendering |
i.MX 8 |
StreamUnlimited Engineering GmbH |
Reference Soundbar with Immersive Audio |
i.MX 8 based embedded hardware module |
StreamUnlimited Engineering GmbH |
Multi-Stream demo showcasing independent music service instances to replicate a connected home environment |
i.MX 8 |
Tata Technologies |
Safe Secure and Scalable, AI Enabled Vehicle HPC Platform with mixed critical workloads and Deterministic communication on NXP iMX95 SoC |
i.MX 95 |
The DiSTI Corporation |
Automotive Cluster / Aircraft Avionics |
i.MX8 QM MEK |
The DiSTI Corporation |
Automotive Cluster / Automotive Infotainment / Medical Monitor |
NXP i.MX95 Toradex Verdin |
TQ Systems GmbH |
Biometric face detection based on the i.MX 93 application processor. The system is be able to recognize known faces independently, even when wearing glasses, a cap, etc. |
MIMX9332XVVXMAB, PCF85063ATL/1,118, PCA9451AHNY, SE97BTP,547, SE050E2HQ1/Z01Z3 |
TQ Systems GmbH |
HMI based on the i.MX 95 application processor. The system displays real-time data from an energy measurement system installed at TQ based on the i.MX 8M Nano |
SE97BTP,547, PCF85063ATL/1,118, PIMX9596AVZXNAB, SE050E2HQ1/Z01Z3, MPF5301AMMA0ES, MPF5302AMMA0ES, PPF0900AMBA1ES |
Truesense srl |
Apnea & Breathing status with Edge AI SW on our UWB module TSRR250 |
SR250 |
Vector Informatik GmbH |
vCANdrive SDV Demonstrator |
NXP i.MX 8 |
VicOne |
AI Guardian, a component of VicOne’s Smart Cockpit Protection solution powered by NXP’s technology, intercepts malicious prompts before they reach the in-cabin AI voice assistant, ensuring that no sensitive data is at risk. |
i.MX 95 |
VicOne |
VicOne’s xCarbon IDPS (Intrusion Detection & Prevention System), equipped with the latest Edge AI, performs inference on cyber risks and ECU anomalies by analyzing various logs and telemetry data through NXP’s OrangeBox. |
OrangeBox |
Follow Us at #NXPCES26
Stay updated on what’s next from NXP and save the date to see us at CES 2026. Follow us on Twitter , Facebook , LinkedIn .