1
Plug It In2
Get Software3
Build, RunSign in to save your progress. Don't have an account? Create one.

Something went wrong! Please try again.
Something went wrong! Please try again.
There are four micro-USB connectors on the board. One each for Full and High Speed USB, one for supplying power only and one for debug. Plug the USB cable into the one labeled +5 V Power Only as shown in the photo.
Something went wrong! Please try again.
Your LPCXpresso55S69 board comes loaded with a program to verify that target MCU is running.
The application is active if the green LED in the RGB-LED flashed with a 1 Hz rate.
Something went wrong! Please try again.
Something went wrong! Please try again.
For this test you need:
OOB_test demo source code is available in SDK.
Something went wrong! Please try again.
The software and tools installation is detailed in two short videos or you can choose to follow the steps below.
 
You can also use the online SDK Builder to create a custom SDK package for the LPC55S69-EVK using the SDK builder The board name for the SDK is LPCXpresso55S69 SDK Builder.
Something went wrong! Please try again.
NXP offers a complimentary toolchain called MCUXpresso IDE.
 Get MCUXpresso IDE
Get MCUXpresso IDE
 
                  Something went wrong! Please try again.
The MCUXpresso Config Tool is an integrated suite of configuration tools that guides users in creating new MCUXpresso SDK projects, and provides pin and clock tools to generate initialization C code for custom board support. It is fully integrated into MCUXpresso or you can download a seperate tool. Click the Get MCUXpresso Config Tools below to get the Config Tools installer.
 
To learn more about the basic interactions between the tools wh working with either an imported MCUXpresso SDK example project or creating a new project within the IDE, watch this three-part video series.
Basic Application Development Using MCUXpresso IDE and MCUXpresso Config Tools
Something went wrong! Please try again.
To set up your LPCXpresso55S69 for use with 3rd party tools, first install LPCScrypt in order to install the board’s device drivers. The video below shows how to use LPCScrypt to program your board’s debug probe using this utility.
Something went wrong! Please try again.
Most of the MCUXpresso SDK examples set up for IAR and Keil tools use the MCU UART for printf output, and this is also an option for the MCUXpresso IDE. If you are not sure how to use a terminal application try one of these tutorials:
Not sure how to use a terminal application? Try one of these tutorials: MCUXpresso Terminal, Tera Term Tutorial, PuTTY Tutorial.
Something went wrong! Please try again.
A short video is provided to walk you through this process or you can follow along the steps below.
The MCUXpresso SDK comes with a long list of example applications code. To see what's available, browse to the SDK boards folder of your SDK installation and select LPCXpresso55S69.
<SDK_Install_Directory>/boards/LPCXpresso55S69
To learn more about specific example code, open the readme.txt file in an example’s directory.
Something went wrong! Please try again.
If one or more of the demo applications or driver examples sounds interesting, you're probably wanting to know how you can build and debug yourself. The Getting Started with MCUXpresso SDK guide provides easy, step-by-step instructions on how to configure, build, and debug demos for all toolchains supported by the SDK.
Use the guide below to learn how to open, build and debug an example application using the MCUXpresso IDE.


The following steps will guide you through opening the hello_world example









 
          


This demo is also available for IAR and KEIL.
The following steps will guide you through opening the hello_world application. These steps may change slightly for other example applications as some of these applications may have additional layers of folders in their path.
If not already done, open the desired example application workspace. Most example application workspace files can be located using the following path:
/boards////iarUsing the hello_world demo as an example, the path is:
/boards/LPCXpresso55S69/demo_apps/hello_world/cm33_core0/iar 
          

 
            Note: In case of building errors, make sure that the correct Board is selected, right click in the project >> Options >> General Options >> Target >> Device, Select the LPC55S69, this board is support in the on IAR Embedded Workbench for Arm version 8.22.2 or Higher.
 
          The LPCXpresso55S69 board comes loaded with the CMSIS-DAP debug interface from the factory. If you have changed the debug LPC-LINK2 application on your board, visit step 2.4 LPCScrypt tutorial in this getting started.




After the MDK tools are installed, Cortex® Microcontroller Software Interface Standard (CMSIS) device packs must be installed to fully support the device from a debug perspective. These packs include things such as memory map information, register definitions and flash programming algorithms. Follow these steps to install the appropriate CMSIS pack.


The following steps will guide you through opening the hello_world application. These steps may change slightly for other example applications as some of these applications may have additional layers of folders in their path.
If not already done, open the desired demo application workspace in:
/boards/////mdkThe workspace file is named .uvmpw, so for this specific example, the actual path is:
/boards/LPCXpresso55S69/demo_apps/hello_world/mdk/hello_world.uvmpwFor example the power manager example project file is here
 
          
J4) is removed when powering the board to boot the debug probe from internal flash 




Something went wrong! Please try again.
Now its time to plug in the board to debug your project:
J4 is removedMore details can be found in the SDK getting started documents found in the SDK folder
<SDK_Install_Directory>/docs/Getting Started with MCUXpresso SDK for LPC55xx.pdfSomething went wrong! Please try again.
Several examples, demos and drivers are available within the SDK to help you get started. Some common examples are listed below:
Something went wrong! Please try again.
The LPC55S69 is secure-by-design and supported by secure software driving the secure System on a Chip (SoC).
| Document | Description | 
|---|---|
| AN12278 LPC55S00 Security Solutions for IoT | This document lays out the differences and advances in the security systems for each LPC55Sxx MCU. | 
| AN12324 LPC55Sxx usage of the PUF and Hash Crypt to AES coding | How to securely generate, store and retrieve user keys using the root key. | 
| AN13094 Using FreeRTOS on LPC55Sxx Series Microcontrollers with TrustZone | How to use FreeRTOS in an ARMv8-M processor that supports TrustZone. | 
| TrustZone with ARMv8-M and the NXP LPC55S69-EVK | An introduction to the ARM TrustZone security feature using MCUXpresso SDK examples and the LPC55S69 EVK. | 
| How to Debug TrustZone Project on MCUXpresso IDE | Introduces debugging TrustZone on the LPCXresso55S69 board using “hello_world” as an example. | 
Several examples, demos and drivers are available within the SDK to help you get started. Some common examples related to security are listed below.
Several simple demonstrations are available in the TrustZone examples including a hello world, secure faults and secure gpio.
Path:
<SDK_PATH>/boards/lpcxpresso55s69/trustzone_examples</SDK_PATH>How to use the PUF controller which provides secure key storage and then sends a secret key via dedicated HW bus directly to Hashcrypt, which uses this key to encrypt data.
Path:
<SDK_PATH>/boards/lpcxpresso55s69/demo_apps_puf_hashcrypt_cryptoA GUI-based application provided to simple generation and provisioning of bootable executables on NXP MCU devices.
| Document | Description | 
|---|---|
| Using ConfigTool to Create USB Project From Start | Creating a USB project with MCUXpresso Config Tool and the LPCXpresso55S69-EVK. | 
Several examples, demos and drivers are available within the SDK to help you get started. Some common examples related to wired communications are listed below.
Demonstrates how to implement a command line shell application.
Path:
<SDK_PATH>/boards/lpcxpresso55s16/demo_apps/shellA number of driver examples exist within the SDK including GPIO, I2C, I2S, SPI and UART.
Path:
<SDK_PATH>/boards/lpcxpresso55s69/driver examplesA number of USB examples for host and device operation exist within the SDK.
Path:
<SDK_PATH>/boards/lpcxpresso55s69/usb_examples| Document | Description | Aplication Note Software | 
|---|---|---|
| AN12805 Establish Secure Connection with Private Cloud | How to create a secure embedded software project with the LPCXpresso55S69 board. | Download | 
| Connecting the LPC55S69 to Amazon Web Services | Demo focused on the WIFI enablement and cloud connectivity through AWS using MCUXpresso and an Amazon Alexa. | - | 
| How to Add Peripherals to AWS IOT and Alexa Skills | Step-by-step approach to adding peripherals to your AWS IOT and Alexa Skills project. | - | 
Several examples, demos and drivers are available within the SDK to help you get started. A common example related to wireless connectivity is listed below.
Shows use of NT3H2111_2211 NTAG I²C plus Connected NFC Tag with I²C Interface Chip and demonstrates basic communication with the device.
Path:
<SDK_PATH>/boards/lpcxpresso55s69/ntag_i2c_plus_examples/ntag_i2C_explorer_blinkThe LPC55S69 platform includes two Arm Cortex-M33 cores running up to 100 MHz. Core 0 includes TrustZone, FPU and two 64-bit Accelerators. The DSP Accelerator is called the PowerQuad DSP co-processor.

| Document | Description | 
|---|---|
| AN12282 Digital Signal Processing for NXP LPC5500 Using PowerQuad | The PowerQuad co-processor is a DSP accelerator that aids the CPU cores in performing mathematical operations such as matrix calculations, filtering, and transform functions, including FFT. | 
| AN12335 LPC55xx/LPC55Sxx Dual Core Communication | The LPC55xx/LPC55Sxx provides a simple hardware means called Inter-CPU Mailbox mechanism for communication. | 
| AN12358 LPC55xx/LPC55Sxx Dual-Core Debug in MCUXpresso | How to debug the asymmetric dual cores of the LPC55S6x. | 
| LPC55xx Multicore Applications with MCUXpresso IDE | How to create, build and debug LPC55xx multicore applications using the LPC55S69-EVK and the MCUXpresso SDK. | 
Several examples, demos and drivers are available within the SDK to help you get started. A common example related to multicore and hardware acceleration is listed below.
Includes how to set up projects for individual cores on a multicore system.
Path:
<SDK_PATH>/boards/lpcxpresso55s69/multicore_examples| Document | Description | 
|---|---|
| AN12939 Implementation of 5.1-channel Audio Solution on LPC55xx | The on-board DSP accelerator makes the LPC55S69 very suitable for USB audio applications. | 
Several examples, demos and drivers are available within the SDK to help you get started. Some common examples related to audio are listed below.
Bare metal and FreeRTOS examples that enumerate a recording or playback device.
USB Device: Audio generator, audio speaker, composite hid audio
USB Host: Audio Speaker
Path:
<SDK_PATH>/boards/lpcxpresso55s69/usb_examplesThe SDK for the LPC55S69 includes graphic examples using the Adafruit TFT LCD shield.
| Software | Description | 
|---|---|
| Graphical User Interfaces for NXP Microcontrollers | Learn more about your GUI options for NXP Microcontrollers. | 
| Open Source LittlevGL GUI Library on Adafruit Touch LCDs with NXP LPC55S69-EVK | Driving Adafruit LDC Display with Capacitive Touch and MCULib. | 
| LVGL Open-Source Graphics Library | LVGL is a free and open-source embedded graphic library with features that enable you to create embedded GUIs with intuitive graphical elements, beautiful visual effects and a low memory footprint. | 
| GUI Guider | A user-friendly graphical user interface development tool from NXP that enables the rapid development of high quality displays with the open-source LVGL graphics library. | 
| NXP emWin Libraries | NXP has partnered with SEGGER Microcontroller to offer the high performance emWin embedded graphics libraries in binary form for free commercial use with any Arm Cortex-M microcontrollers from NXP. | 
| GUI Development With emWin and AppWizard | How to use the different features in AppWizard to create complete, ready-to-run projects based on emWin. | 
Several examples, demos and drivers are available within the SDK to help you get started. Some common examples related to display and graphics are listed below.
A demo application to show littlevgl widgets.
Path:
<SDK_PATH>/boards/lpcxpresso55s69/littlevgl_examplesDemonstrates the graphical widgets of the emWin library.
Path:
<SDK_PATH>/boards/lpcxpresso55s69/emwin_gui_demo| Document | Description | Application Note Software | 
|---|---|---|
| AN12868 Camera Interface in LPC55(S)xx | Introduces the camera interface, features and API routines and demo. | Download | 
| Document | Description | 
|---|---|
| FreeMASTER How To | A starting guide for engineers using FreeMASTER tool. | 
| FreeMASTER 3.0 - Installation Guide | This article will walk you through the installation process of FreeMASTER 3.0. | 
| FreeMASTER Four-Part Webinar Series | On-demand training provides an overview of the FreeMASTER software, its features, capabilities, available examples, application use cases and how to easily get started. | 
Several examples, demos and drivers are available within the SDK to help you get started. Some common examples related to Motor Control are listed below.
Path:
<SDK_PATH>/middleware/motor_controlWatch variables and graphs over various interface options.
Path:
<SDK_PATH>/boards/lpcxpresso55s69/freemaster_examplesDescribes the embedded-side software driver which implements a serial interface between the application and the host PC and covers the native Serial UART communication and CAN communication for the applicable devices.
Path:
<SDK_PATH>/middleware/freemaster/doc/user_guide
| Training | Description | 
|---|---|
| Basic Application Development Using MCUXpresso IDE and MCUXpresso Config Tools | This three-part video series covers the basic interactions between the MCUXpresso IDE and Config Tools when working with either an imported SDK example project or creating a new one. | 
| LPC55s6X Training | Full list of on-demand training, how-to videos and webinars from NXP about this product. | 
Connect with other engineers and get expert advice on designing with the LPC55 family on one of our community sites.
Plug It In and Demo of LPC55S69
Get Familiar with the Board
Attach the USB Cable
Run the Out-of-the-Box Demo
Switch and LED Test
Audio Test
Jump Start Your Design with the MCUXpresso SDK
Install Your Toolchain
MCUXpresso Config Tools
Debug Probe Firmware Update Using LPCScrypt
Serial Terminal