Getting Started with the MCIMX7SABRE

Last Modified: 2019-03-18 10:59:15Supports i.MX 7Dual SABRE Board

Contents of this document

  • 1

    Out of the Box
  • 2

    Embedded Linux®
  • 3

    Embedded Android
  • 4

    FreeRTOS
  • 5

    Explore

1. Out of the Box

The following section describes the steps to boot the i.MX7Dual Sabre.

Development Kit Contains:

  • i.MX7Dual Sabre board for smart devices
  • USB cable (micro-B to standard-A)
  • Cable -Assembly, USB 3.0 Type-A Male, USB micro-B Male, Shielded, 1m
  • 5V/5A universal power supply
  • Quick Start Guide
  • 8 GB SD Card with bootable operating system demonstration image

1.1 Get Familiar with the Board

GS-RDIMX7DSABREBRD-IMG1

Figure 1. i.MX7Dual Sabre front

GS-RDIMX7DSABREBRD-IMG2

Figure 2. i.MX7Dual Sabre back

1.2 Insert the SD Card (SD1/J6)

The kit includes an SD card with a pre-built NXP Linux binary demo image. Without modifying the binary inside the SD card, booting from this SD card provides a default system with certain features for building other applications on top of Linux. The software is described in the following sections.

1.3 Connect USB Debug Cable

Connect the micro-B end of the supplied USB cable into Debug UART port J11. Connect the other end of the cable to a host computer.

If you are not sure about how to use a terminal application, try one of the following tutorials depending on the operating system of the host machine:

Tera Term Tutorial, PuTTY Tutorial, Minicom Tutorial.

1.4 Connect the HDMI cable

To see the user interface provided with the SD card image binary connect a monitor via the HDMI connector (J9).

1.5 Boot Switch Setup

Click here to see the Boot Switch Setup

1.6 Connect Power Supply

Connect the 5V power supply cable to the 5V DC power jack (J1).

Power the board by flipping the switch (SW1). The processor starts executing from the on-chip ROM code. With the default boot switch setup, the code reads the fuses to define the media where it is expected to have a bootable image. After it finds a bootable image on the SD card, the U-Boot execution should begin automatically.

Information is printed in the smaller number serial console for the Cortex-A7 (COM9 on Windows as an example and /dev/ttyUSB* on Linux). If you don not stop the U-Boot process, it continues to boot the Linux kernel.

On Windows as an example

1.7 Congratulations Linux® has booted

Once Linux is booted, login using the user name root and no password.

Tip: To proceed to U-Boot, press any key before the value of the U-Boot environment variable, bootdelay, decreases and before it times out (default 3 seconds). If you stop the U-Boot process, you can run the following command to continue with the Linux boot process:

# boot

2. Embedded Linux®

This section is applicable ONLY if attempting to load a Linux operating system on the board.

The i.MX Linux Board Support Package (BSP) is a collection of binary files, source code, and support files that are used to boot an Embedded Linux image on a specific i.MX development platform.

Current releases of Linux binary demo files can be found on the i.MX Linux download page. The Linux User Guide and Linux Reference Manual provide additional information. Additional documentation can be found the i.MX Linux documentation bundle, or under the Linux sections on the i.MX Software and Development Tool.

2.1 Overview

Before the Linux OS kernel can boot on an i.MX board, the Linux image is copied to a boot device (SD card, eMMC and so on) and the boot switches are set to boot that device.

There are various ways to download the Linux BSP image for different boards and boot devices.

For this getting started guide, only a few methods to transfer the Linux BSP image to an SD card are listed. Experienced Linux developers can explore other options.

2.2 Download an NXP Linux BSP pre-built image

The latest pre-built images for the i.MX 8QuadMax MEK are available on the Linux download page. The file L4.14.78_1.0.0_ga_images_MX7DSABRESD.zip gathers every artifact required to boot the board.

The pre-built NXP Linux binary demo image provides a typical system and basic set of features for using and evaluating the processor. Without modifying the system, the users can evaluate hardware interfaces, test SoC features, and run user space applications.

When more flexibility is desired, an SD card can be loaded with individual components (boot loader, kernel, dtb file, and rootfs file) one-by-one or the .sdcard image is loaded and the individual parts are overwritten with the specific components.

2.3 Burn NXP Linux BSP image using UUU

In addition to the connections from Out of box chapter, connect the J25 to the host machine using the proper USB cable.

Turn off the board. Consult Boot switch setup and configure the board to boot on SDP (Serial Download Protocol) mode.

Depending on the OS used in the host machine, the way to transfer the Linux BSP image onto an SD card can vary.

Choose an option below for detailed instructions:

3. Embedded Android

This section describes the boot process of loading the i.MX7Dual Sabre board with an Embedded Android system image and introduces how to build the software components that create your own system image. For details on building the Android platform, see https://source.android.com/source/building.html

The current release includes Demo Images, Source code and Documentation. These can also be found under Android section of the i.MX Software and Development Tool.

3.1 Overview

The storage devices on the development system (MMC/SD or NAND) must be programmed with the U-Boot boot loader. The boot process determines which storage device to access based on the switch settings. When the boot loader is loaded and begins execution, the U-Boot environment space is then read to determine how to proceed with the boot process.

The images can come from pre-built release packages or be created from source code. Regardless of how you obtain them, all Android images contain the following components:

  • U-Boot image: u-boot.imx

  • boot image: boot.img

  • Android system root image: system.img

  • Recovery root image: recovery.img

For more information about the Android BSP refer to the Android User Guide.

Depending on the OS used in the host machine, the way to transfer the Android BSP image onto an SD card can vary.

3.2 Download NXP Android BSP image

The pre-built NXP Android demo image provides a default system with certain features for evaluation. Without modifying the system, users can perform some basic operations, and interact with the system to test hardware interfaces and develop software application in the user space.

The pre-built images from the package are categorized by boot device and put in the directory with the device name. The latest pre-built image files can be found in Android section on the i.MX Software and Development Tool, or on the demo images downloader link.

Burn NXP Android BSP image using UUU

In addition to the connections from Out of box chapter, connect the J25 to the host machine using the proper USB cable.

Turn off the board. Consult Boot switch setup and configure the board to boot on SDP (Serial Download Protocol) mode.

Depending on the OS used in the host machine, the way to transfer the Linux BSP image onto an SD card can vary.

Choose an option below for detailed instructions:

4. FreeRTOS

This section describes how to load FreeRTOS for i.MX7Dual. FreeRTOS is an optional Real-Time Operating System (RTOS) which NXP uses to enable the Cortex-M cores in some of our products. Enabling the Cortex-M cores is an optional step. If you do not wish to enable the Cortex-M4 on i.MX7Dual at this moment you can skip this section.

The FreeRTOS BSP for i.MX7Dual is a suite of robust peripheral drivers and multicore communication mechanism designed to simplify and accelerate application development on the i.MX7Dual Processor.

Included in the FreeRTOS BSP for i.MX7Dual is full source code under a permissive open-source license for all demos, examples, middleware, and peripheral driver software.

4.1 Overview

The FreeRTOS BSP for i.MX7Dual consists of the following runtime software components written in C:

  • Arm® Cortex Microcontroller Software Interface Standard (CMSIS) Core, DSP standard libraries, and CMSIS-compliant device header files which provide direct access to the peripheral registers and bits.
  • A set of peripheral drivers that provides a simple, stateless driver with an API encapsulating register access of the peripheral.
  • A multicore communication mechanism (RPMsg) to decrease the developing difficulty of multicore communication.
  • A FreeRTOS operating system to provide an event triggered preemptive scheduling RTOS.

The demos/examples in FreeRTOS BSP are built for on-chip Tightly Coupled Memory (TCM) in the Arm® Cortex®-M4® core.

4.2 Download NXP FreeRTOS source and demos

Current releases of the NXP FreeRTOS BSP and source code can be found on the links below. There is option to download a self-extract installer that can be used on Windows OS, or a tarball for installation on Linux OS.

There are four main areas under the install directory of the FreeRTOS BSP tree used to provide the full source code for each demo application:

GS-RDIMX7DSABREBRD-IMG3
  • The examples folder contains all demos/examples source code and board configuration files. All 21 applications are cataloged by board name.
  • The middleware folder contains the source code of all the middleware used by demos and examples. The open source multicore communication stack – RPMsg is included in the middleware folder.
  • The platform folder contains the source code for the primary components including CMSIS header files, peripheral drivers, startup, utilities, and linker files.
  • The rtos folder contains the source code of market leading RTOS – FreeRTOS OS.

The FreeRTOS BSP comes with rich demo applications and driver examples. To see what’s available, browse the BSP examples folder and select the i.MX7Dual Sabre board
(/examples/imx7d_sdb_m4/demo_apps//).

To learn more about demo applications or driver examples, open the FreeRTOS i.MX7Dual Demo Application User’s Guide, located in /doc.

If one or more of the demo applications or driver examples sounds interesting, you’re probably wanting to know how you can build and debug yourself. The Getting Started Guide with FreeRTOS BSP provides easy, step-by-step instructions on how to configure, build, and debug demos for all toolchains supported by the BSP.

Depending on the OS used in the host machine, the way to build and deploy the demos can vary.

The pre-built NXP Android demo image provides a default system with certain features for evaluation. Without modifying the system, users can perform some basic operations, and interact with the system to test hardware interfaces and develop software application in the user space.

The pre-built images from the package are categorized by boot device and put in the directory with the device name. The latest pre-built image files can be found in Android section on the i.MX Software and Development Tool, or on the demo images downloader link.

Burn NXP Android BSP image using UUU

In addition to the connections from Out of box chapter, connect the J25 to the host machine using the proper USB cable.

Turn off the board. Consult Boot switch setup and configure the board to boot on SDP (Serial Download Protocol) mode.

Depending on the OS used in the host machine, the way to transfer the Linux BSP image onto an SD card can vary.

Choose an option below for detailed instructions:

4.3 Run applications using U-Boot

This section describes how to run applications using an SD card using pre-built U-Boot image for i.MX processor.

  1. Prepare an SD card with a pre-built U-Boot + Linux image from Linux BSP package for the i.MX7Dual processor following the steps on the Embedded Linux® tab. If you have already loaded your SD card with a Linux image you can skip this step.
  2. Insert the SD card to the your host computer (Linux or Windows), and copy the application image (for example hello_world.bin) that you want run to the FAT partition of the SD card.
  3. Safely remove the SD card from the PC.
  4. Insert the SD card to the target board. Make sure to use the default boot SD slot and double check the Boot Switch Setup. The default configuration of the validation board boots from SD1/J6, and on Sabre board there is only one SD slot which is used for boot.
  5. Connect the DEBUG UART slot on the board with your PC through the USB cable. The Windows OS installs the USB driver automatically, and the Ubuntu OS will find the serial devices as well.

    See Serial Communication Console setup section in Out of the Box for more instructions for serial communication applications.

  6. Open a second terminal emulator on the i.MX7Dual Sabre board’s second enumerated serial port. This is the Cortex-M4’s serial console. Set the speed to 115200 bps, data bits 8, no parity, and power on the board.
  7. Power up the board and stop the boot process by pressing any key before the U-boot countdown reaches zero. At the U-Boot prompt on the first terminal emulator, type the following commands to U-Boot.

    • => fatload mmc 2:1 0x7F8000 .bin

    • => dcache flush

    • => bootaux 0x7F8000

These commands copy the FreeRTOS memory image file from the first partition of the SD card into the Cortex-M4’s memory and releases the Cortex-M4 from reset.

Some applications with the names ended by ddr or ocram in FreeRTOS BSP should be run in DDR or OCRAM. Those ended by qspi should boot from external QSPI flash.

For additional instructions on how to boot from other storage, read section 6.2 and 6.3 in Getting Started with FreeRTOS found inside the package downloaded in section Download NXP FreeRTOS source and demos.

Example Demo

Demo and example applications are provided to demonstrate peripheral drivers, FreeRTOS kernel, RPMsg usage and to highlight the main features of the i.MX7Dual processor.

The FreeRTOS BSP provides two types of software applications:

4.4 Cortex-M4 standalone sensor demo:

The Sensor Demo i.MX7Dual is a simple demonstration program that uses the FreeRTOS and a set of drivers provided by NXP. It can get the current gravitational acceleration, temperature, altitude and magnetic field strength of the board. The purpose of this demo is to show how to use the I2C driver as a Controller to communicate with other I2C Targets.

In the second terminal emulator for Cortex-M4, you should see text indicating the sensor example is running (e.g., below). Choose one of the sensor demos and affect the given sensor by moving the board or moving something magnetic near it.

-------------- iMX7D SDB on board sensor example --------------

Please select the sensor demo you want to run:
[1].FXAS21002 3-axes Gyro sensor
[2].FXOS8700 6-axes Acc+Mag sensor
[3].MPL3115 Pressure sensor

4.5 Cortex-A7/Cortex-M4 RPMsg Ping Pong demo

This demo application demonstrates the RPMsg remote stack working on FreeRTOS OS. It works with Linux RPMsg controller peer to transfer integer values back and forth.

The name service handshake is performed first to create the communication channels.

Next, Linux OS transfers the first integer to FreeRTOS OS. The receiving peer adds 1 to the integer and transfers it back. The loop continues to demonstrate the stability of RPMsg stack.

Immediately messages will start printing on each console.

  1. To run this demo, load the FreeRTOS binary to the Cortex-M4 following section Run applications using U-Boot. On U-Boot, change the fdt_file to enable the M4 core on kernel then run the boot command:

    => setenv fdt_file imx7d-sdb-m4.dtb

    => boot

  2. On Linux user space, probe the imx_rpmsg_pingpong module to start the communication between the cores:

    Linux side:

    root@imx7dsabresd:~# modprobe imx_rpmsg_pingpong
    imx_rpmsg_pingpong rpmsg0: new channel: 0x400 -> 0x1!
    root@imx7dsabresd:~# get 1 (src: 0x1)
    get 3 (src: 0x1)
    get 5 (src: 0x1)
    get 7 (src: 0x1)
    get 9 (src: 0x1)
    get 11 (src: 0x1)

  3. FreeRTOS side:

    Name service handshake is done, M4 has setup a rpmsg channel [1 ---> 1024]
    Get Data From A7 : 0
    Get Data From A7 : 2
    Get Data From A7 : 4
    Get Data From A7 : 6
    Get Data From A7 : 8
    Get Data From A7 : 10

  4. The cores exchange messages with each other until the demo stops.

5. Explore

5.1 Explore the documentation

When working with embedded systems, it is important to bear in mind that the documentation is wide and diverse. It is common to have different levels of documentation. The i.MX7Dual Sabre board has some documents. However, this board’s processor is i.MX7Dual which is documented with SoC level documents. The BSPs available are documented with the BSP level documents.

Choose an option below for related documents:

5.2 Board documentation

5.3 SoC documentation

In the case of i.MX7Dual SoC the following documents are available.

Table 5. List of i.MX7Dual chip-related documents

Document Description
i.MX7Dual DataSheet Describes the SoC physical and electrical characteristics, the part number meaning.
i.MX7Dual Reference Manual Lists what the SoC supports, the registers and the memory map. Describes the features, workflow, the boot flow, and the meaning of each register’s bits.
List the hardware issues for that SoC. It may be an Arm core or an i.MX core issue. It may or may not have a workaround.
i.MX7Dual Security Reference Manual Sing-in to request access to the i.MX7Dual Security Reference Manual. The link to download is sent in the email.

5.4 Software documentation

For i.MX7Dual Sabre the following BSPs are available.

  • Linux Kernel distribution using the Yocto Project (L4.9.88_2.0.0): For details, see the documentation in i.MX7Dual Sabre BSP Linux documents
  • Android (imx-o8.0.0_1.0.0_ga): For details, see the documentation in i.MX7Dual Sabre BSP Android documents
  • FreeRTOS (1.0.1): For details, see the documentation in i.MX7Dual Sabre BSP FreeRTOS documents

Each BSP has a set of documents, in the next tables all the BSP documentation is described. The order the documents appear in the table is the recommended read order.

Table 6. i.MX7Dual Sabre BSP Linux documents

Document Description
L4.9.88_2.0.0 Doc Bundle Downloads all the i.MX Linux BSP files listed here as one tarball.
i.MX Linux Release Notes If you do not know where to start, start here! It lists the supported boards, the supported features, the packages versions and the known issue list.
i.MX Linux Users Guide Describes the steps to download, build and deploy the i.MX Linux BSP. For example, detail how to configure, build, and deploy U-Boot booting from different medias.
i.MX Yocto Project Users Guide Linux Describes the steps to download, build, deploy and configure the Yocto Project metadata, and build an image.
i.MX BSP Porting Guide Linux Describes the steps to port the i.MX Linux BSP to a custom board or platform.
i.MX Reference Manual Linux Describes the i.MX BSP Linux Kernel drivers, features, and how to configure the kernel. It also describes how drivers works.
i.MX Graphics Users Guide Linux Describes how to test and configure the GPU for custom use cases.

Table 7. i.MX7Dual Sabre BSP Android documents

Document Description
imx-o8.0.0_1.0.0_ga Doc Bundle Downloads all the i.MX Android BSP files listed here as one tarball.
Android Release Notes If you do not know where to start, start here! It lists the supported boards, the supported features, the packages version, and the known issue list.
Android Quick Start Guide Describes the board, the files in the i.MX Android BSP, how to deploy and foot the images using different displays.
Android Users Guide It is the document with instructions on how to set a Linux machine to build Android, how to build, configure, and, deploy the i.MX Android BSP.
Describes the steps to port the i.MX Android BSP to a custom board or platform; including steps to configure multimedia and display.
i.MX Graphics Users Guide Android Describes how to test and configure the GPU for custom use cases.
Android Frequently Asked Questions Lists frequently asked question related to Android.

Table 8. i.MX7Dual Sabre BSP FreeRTOS documents

Document Description
FreeRTOS Bundle for Linux Download the i.MX FreeRTOS BSP for Linux host. The documentation is available in the folder doc/.
Download the i.MX FreeRTOS BSP for Windows host. The available documentation is available in the folder doc/.

5.6 Key features in Linux BSP

With Linux running on the i.MX board, you can evaluate special features that i.MX SoCs provide. This tutorial present the step-by-step for the following demos.

Choose an option below for detailed instructions:

5.7 Power management

This example shows how to suspend to low-power modes and resuming to normal operation.

  • Enter the command below in order to enable serial TTY as a wake up source for the board:

    # echo enabled > /sys/class/tty/ttymxc0/power/wakeup

  • Enter the command below to enter Suspend-To-RAM mode:

    # echo mem > /sys/power/state
    PM: Syncing filesystems ... done.
    Freezing user space processes ... (elapsed 0.005 seconds) done.
    Freezing remaining freezable tasks ... (elapsed 0.001 seconds) done.
    Suspending console(s) (use no_console_suspend to debug)

  • Press any key on the keyboard to wake up the board. The following messages should appear on terminal:

    PM: suspend of devices complete after 637.926 msecs
    PM: suspend devices took 0.640 seconds
    PM: late suspend of devices complete after 1.966 msecs
    PM: noirq suspend of devices complete after 1.864 msecs
    Disabling non-boot CPUs ...
    PM: noirq resume of devices complete after 1.104 msecs PM: resume of devices complete after 99.689 msecs PM: resume devices took 0.110 seconds Restarting tasks ... done.

5.8 Multimedia - Simple audio example

Connect your earphone to the Audio Jack on the i.MX7Dual Sabre board.

If your earphone includes a microphone feature (TRRS with four contacts), do not push the microphone jack to the end. Leave one contact ring outside.

# gst-launch-1.0 audiotestsrc ! alsasink
Setting pipeline to PAUSED ...
Pipeline is PREROLLING ...
Pipeline is PREROLLED ...
Disabling non-boot CPUs ...
Setting pipeline to PLAYING ... New clock: GstAudioSinkClock

You should be able to listen a tone on the earphone.

When you are done with the tone, finish the command line by pressing kbd:[Ctrl+C]

This example is very simple. It shows the link between audiotestsrc and alsasink.

5.9 Decoder video audio

This example explains how to decode just the audio from a video file. Copy a video file to your /home/root/ on your SD card rootfs partition, boot the board from the SD card and run the command below:

Note: You can obtain the file used in the example for free from the Big Buck Bunny site.

# gst-launch-1.0 filesrc location=Big_Bucky_Bunny.mov ! qtdemux \
! beepdec ! alsasink
Setting pipeline to PAUSED ...
Pipeline is PREROLLING ...
====== BEEP: 4.0.9 build on Sep 22 2016 18:44:36. ======
file: /usr/lib/imx-mm/audio-codec/wrap/lib_mp3d_wrap_arm12_elinux.so.3 CODEC: BLN_MAD-MMCODECS_MP3D_Arm_02.13.00_CORTEX-A8 build on Apr 10 2014 15:26:15. Pipeline is PREROLLED ... Setting pipeline to PLAYING ... New clock: GstAudioSinkClock

5.10 Security

This example shows the advantages of using CAAM as an encryption offload engine provided by NXP.

5.11 CAAM and CryptoDev

As many of the i.MX NXP processors, i.MX7Dual Sabre board. includes the Cryptographic Acceleration And Assurance Module CAAM module that can be used through CryptoDev in order to accelerate by hardware the encryption and decryption process. It is recommended to use this module when working with large amounts of data or in any application where performance is important.

5.12 Checking the speed performance

OpenSSL is an open source project that defines the security protocols SSL (Secure Sockets Layer) and TLS (Transport Layer Security). It has a software library that can be used in applications that requires a secure information transmission in order to prevent eavesdropping.

OpenSSL includes a speed command that tests the encryption performance for a desired encryption algorithm. For this example the algorithm used is the aes-128-cbc that implements the Advanced Encryption Standard (AES) encryption algorithm, with a Cipher Block Chaining (CBC) mode of operation and 128 bits block.

The OpenSSL speed test can be seen using the following command:

# openssl speed -evp aes-128-cbc
Doing aes-128-cbc for 3s on 16 size blocks: 3992233 aes-128-cbc's in 3.00s
Doing aes-128-cbc for 3s on 64 size blocks: 1151356 aes-128-cbc's in 3.00s
Doing aes-128-cbc for 3s on 256 size blocks: 299139 aes-128-cbc's in 3.00s
Doing aes-128-cbc for 3s on 1024 size blocks: 75534 aes-128-cbc's in 3.00s
Doing aes-128-cbc for 3s on 8192 size blocks: 9469 aes-128-cbc's in 2.99s
OpenSSL 1.0.2d 9 Jul 2015
built on: reproducible build, date unspecified
options:bn(64,32) rc4(ptr,char) des(idx,cisc,16,long) aes(partial) idea(int) blowfish(ptr)
compiler: arm-poky-linux-gnueabi-gcc -march=armv7-a -mfloat-abi=hard -mfpu=neon -mtune=cortex-a7 --sysroot=/home/bamboo/buM
The 'numbers' are in 1000s of bytes per second processed. type 16 bytes 64 bytes 256 bytes 1024 bytes 8192 bytes aes-128-cbc 21291.91k 24562.26k 25526.53k 25782.27k 25943.16k

Load the cryptodev module and run the openssl command again. This time you should be able to see that the timing values show the accelerated values. As the block sizes increases, the elapsed time decreases:

# modprobe cryptodev
cryptodev: driver 1.8 loaded.
root@imx6ulevk:~# openssl speed -evp aes-128-cbc -engine cryptodev
engine "cryptodev" set.
Doing aes-128-cbc for 3s on 16 size blocks: 91936 aes-128-cbc's in 0.14s
Doing aes-128-cbc for 3s on 64 size blocks: 88205 aes-128-cbc's in 0.15s
Doing aes-128-cbc for 3s on 256 size blocks: 70223 aes-128-cbc's in 0.09s
Doing aes-128-cbc for 3s on 1024 size blocks: 50836 aes-128-cbc's in 0.10s
Doing aes-128-cbc for 3s on 8192 size blocks: 11174 aes-128-cbc's in 0.03s
OpenSSL 1.0.2d 9 Jul 2015
built on: reproducible build, date unspecified
options:bn(64,32) rc4(ptr,char) des(idx,cisc,16,long) aes(partial) idea(int) blowfish(ptr)
compiler: arm-poky-linux-gnueabi-gcc -march=armv7-a -mfloat-abi=hard -mfpu=neon-mtune=cortex-a7 --sysroot=/home/bamboo/buM
The 'numbers' are in 1000s of bytes per second processed. type 16 bytes 64 bytes 256 bytes 1024 bytes 8192 bytes aes-128-cbc 10506.97k 37634.13k 199745.42k 520560.64k 3051246.93k

The encryption algorithms supported by the CryptoDev can be listed by the following command:

# openssl engine cryptodev -c
(cryptodev) BSD cryptodev engine
[RSA, DSA, DH, DES-CBC, DES-EDE3-CBC, AES-128-CBC, AES-192-CBC, AES-256-CBC, hmacWithMD5, hmacWithSH A1, RIPEMD160, MD5, SHA1]

5.13 Connectivity

To connect to the Internet on Linux with your i.MX7Dual Sabre follow the steps below:

  • Connect a Ethernet cable to the board RJ-45 connector.

  • Boot up the board and wait for the Linux prompt.

  • On the board, enter the following command:

    # ifconfig eth0
  • Ping any site to corroborate functionality

    # ping 8.8.8.8
    PING 8.8.8.8 (8.8.8.8) 56(84) bytes of data.
    64 bytes from 8.8.8.8: icmp_seq=1 ttl=56 time=9.22 ms
    64 bytes from 8.8.8.8: icmp_seq=2 ttl=56 time=6.13 ms
    64 bytes from 8.8.8.8: icmp_seq=3 ttl=56 time=6.30 ms
    64 bytes from 8.8.8.8: icmp_seq=4 ttl=56 time=9.26 ms

Tera Term Tutorial

Tera Term Tutorial

Tera Term is a very popular open source terminal emulation application. This program can be used to display information sent from your NXP development platform's virtual serial port.

  • Download Tera Term from SourceForge. After the download, run the installer and then return to this webpage to continue.

    Download

  • Launch Tera Term. The first time it launches, it will show you the following dialog. Select the serial option. Assuming your board is plugged in, there should be a COM port automatically populated in the list. Get Started with MC56F80000-EVK
  • Configure the serial port settings (using the COM port number identified earlier) to 115200 baud rate, 8 data bits, no parity and 1 stop bit. To do this, go to Setup -> Serial Port and change the settings.
  • Verify that the connection is open. If connected, Tera Term will show something like below in its title bar Get Started with MC56F80000-EVK
  • You're ready to go

PuTTY Tutorial

PuTTY Tutorial

PuTTY is a popular terminal emulation application. This program can be used to display information sent from your NXP development platform's virtual serial port.

  • Download PuTTY using the button below. After the download, run the installer and then return to this webpage to continue.

    Download

  • PuTTY by either double-clicking on the *.exe file you downloaded or from the Start menu, depending on the type of download you selected Get Started with MC56F80000-EVK
  • Click Open to open the serial connection. Assuming the board is connected and you entered the correct COM port, the terminal window will open. If the configuration is not correct, PuTTY will alert you
  • You're ready to go

Minicom Tutorial

Minicom Tutorial

Serial communication console setup

On the command prompt of the Linux host machine, run the following command to determine the port number:

$ ls /dev/ttyUSB*

The smaller number is for Cortex-A7 and the bigger number is for Cortex-M4.

Minicom

Use the following commands to install and run the serial communication program (minicom as an example):

  1. Install Minicom using Ubuntu package manager. $ ls /dev/ttyUSB*
  2. Launch Minicom using a console window using the port number determined earlier. $ sudo minicom /dev/ttyUSB* -s
  3. Configure Minicom as show in [Minicom Configuration]
  4. GS-MCIMX7SABRE-MINICOM

    Figure 3. Minicom Configuration

  5. The next step is to [Connect the HDMI cable].