1
Plug It In2
Get Software3
Build, RunSign in to save your progress. Don't have an account? Create one.
Let's take your MIMXRT1170-EVK for a test drive, You have the choice of watching the sequence in a short video or following the detailed actions listed below.
Something went wrong! Please try again.
Plug the power adapter wire into the MIMXRT1170-EVK board 5V DC IN header (J43
) and switch on 5V DC IN (SW5
).
Something went wrong! Please try again.
The MIMXRT1170-EVK board comes preprogrammed with a demo that will initiate the LED on the board to flash when plugged in.
When the board is tilted, the green LED gradually illuminates based on the degree of tilt on the X-axis.
Something went wrong! Please try again.
Something went wrong! Please try again.
The MCUXpresso software development kit (SDK) is complimentary and includes full source code under a permissive open-source license for all hardware abstraction and peripheral driver software.
Click below to download the latest SDK release for the MIMXRT1170-EVK, make sure you select Host OS, Toolchain and desired components.
Something went wrong! Please try again.
MCUXpresso IDE is development platform ecosystem from NXP. It provides an end-to-end solution enabling engineers to develop embedded applications from initial evaluation to final production.
Want to use a different toolchain? Need help choosing?
Something went wrong! Please try again.
The MCUXpresso Config Tool is an integrated suite of configuration tools that guides users in creating new MCUXpresso SDK projects, and also provides pin and clock tools to generate initialization C code for custom board support. It is fully integrated into MCUXpresso or you can download it as a separate tool.
Something went wrong! Please try again.
Many of the example applications output data over the MCU UART so you'll want to make sure that the driver for the board's virtual COM port is installed. Before you run the driver installer, you MUST have the board plugged into your PC.
Download driverSomething went wrong! Please try again.
Install and configure your preferred terminal software to 115200 baud rate, 8 data bits, no parity and 1 stop bit. To determine the port number of the MIMXRT1170-EVK’s virtual COM port, open the device manager and look under the "Ports" group.”.
Not sure how to use a terminal application? Try one of these tutorials: MCUXpresso IDE Terminal Tutorial, Tera Term Tutorial, PuTTY Tutorial.
Something went wrong! Please try again.
Something went wrong! Please try again.
The MCUXpresso SDK comes with a long list of example applications code. To see what's available, browse to the SDK boards folder of your SDK installation and select MIMXRT1170-EVK.
<SDK_Install_Directory>/boards/evkmimxrt1170
To learn more about specific example code, open the readme.txt file in an example’s directory.
Something went wrong! Please try again.
If one or more of the demo application or driver examples sounds interesting, you probably want to know how you can build and debug it yourself. The Getting Started with SDK guide provides easy, step-by-step instructions on how to configure, build and debug demos for all toolchains supported by the SDK.
Use the guide below to learn how to open, build and debug an example application in MCUXpresso IDE, IAR Embedded Workbench IDE, Keil MDK or Arm GCC.
Multicore application projects consist of two (or more) linked projects – one project containing the Master code and the other project(s) containing the Slave code. The ‘Master’ project contains a link to the ‘Slave’ project, which will cause the output image from the ‘Slave’ to be included into the ‘Master’ image when the Master project is built. Building the Master project will trigger the Slave project to be built first.
The RT1170 SDK provides a collection of Multicore example applications. Each Multicore example has two source directories, one for the Arm CM7 and one for the Arm CM4.
The following steps will guide you through the Multicore Hello World application using MCUXpresso IDE.
Note: The MCUXpresso IDE installation can be found at the section “2. Get Software” of the Getting Started website.
To download and run the application, perform these steps:
SW1
is set to 0010 to boot from QSPIJ43
(if J38
is set to [1-2])J11
portRefer to the Getting Started with MCUXpresso SDK for MIMXRT1170-EVK.pdf in the <SDK install folder>/docs folder from the SDK for additional information and instructions to build and run example applications.
The following steps will guide you through opening the hello_world application. These steps may change slightly for other example applications as some of these applications may have additional layers of folders in their path.
<sdk_dir>/boards/<sdk_board_name>/<example_type>/<application_name>/<core_type>/iar
Using the hello_world demo as an example, the path is:
<sdkl_dir>/boards/evkmimxrt1170/demo_apps/hello_world/cm7/iar/hello_world.eww
Note: In case of building errors, make sure that the correct Board is selected, right click in the project >> Options >> General Options >> Target >> Device, Select the NXP MIMXRT1176xxxA_M7, this board is supported in IAR Embedded Workbench for Arm version 8.50.6 or Higher.
To download and run the application, perform these steps:
SW1
is set to 0010 to boot from QSPIJ43
(if J38
is set to [1-2])J11
portRefer to the Getting Started with MCUXpresso SDK for MIMXRT1170-EVK.pdf in the <SDK install folder>/docs folder from the SDK for additional information and instructions to build and run multicore example applications.
After the MDK tools are installed, Cortex® Microcontroller Software Interface Standard (CMSIS) device packs must be installed to fully support the device from a debug perspective. These packs include things such as memory map information, register definitions and flash programming algorithms. Follow these steps to install the appropriate CMSIS pack.
The following steps will guide you through opening the hello_world_demo_cm7 application.
<install_dir>/boards/<board_name>/<example_type>/<application_name>/mdk
The workspace file is named as <demo_name>.uvmpw. For this specific example, the actual path is:
<install_dir>/boards/evkmimxrt1170/demo_apps/hello_world/cm7/mdk/hello_world_demo_cm7.uvmpw
This section describes steps to run a demo application using J-Link GDB Server application. To perform this exercise, make sure that either:
To download and run the application, perform these steps:
SW1
is set to 0010 to boot from QSPIJ43
(if J38
is set to [1-2])J11
portRefer to the Getting Started with MCUXpresso SDK for MIMXRT1170-EVK.pdf in the <SDK install folder>/docs folder from the SDK for additional information and instructions to build and run multicore example applications.
This section contains the steps to install the necessary components required to build and run an MCUXpresso SDK demo application with the Arm GCC toolchain, as supported by the MCUXpresso SDK. There are many ways to use Arm GCC tools, but this example focuses on a Windows environment. Though not discussed here, GCC tools can also be used with both Linux OS and Mac OSX.
Download and run the installer from launchpad.net/gcc-arm-embedded
. This is the actual toolset (in other words, compiler, linker, etc.). The GCC toolchain should correspond to the latest supported version, as described in MCUXpresso SDK Release Notes Supporting MIMXRT1170-EVK from <SDK>/docs folder.
The Minimalist GNU for Windows (MinGW) development tools provide a set of tools that are not dependent on third party C-Runtime DLLs (such as Cygwin). The build environment used by the MCUXpresso SDK does not utilize the MinGW build tools but does leverage the base install of both MinGW and MSYS. MSYS provides a basic shell with a Unix-like interface and tools.
sourceforge.net/projects/mingw/files/Installer/
.Note: The installation path cannot contain any spaces.
<mingw_install_dir>\bin
Assuming the default installation path, C:\MinGW
, an example is shown below. If the path is not set correctly, the toolchain does not work.
Note: If you have C:\MinGW\msys\x.x\bin
in your PATH variable (as required by KSDK 1.0.0), remove it to ensure that the new GCC build system works correctly.
Create a new system environment variable and name it ARMGCC_DIR. The value of this variable should point to the Arm GCC Embedded tool chain installation path, which, for this example, is:
C:\Program Files (x86)\GNU Tools ARM Embedded\<version>
Reference the installation folder of the GNU Arm GCC Embedded tools for the exact path name of your installation.
To build an example application, follow these steps.
<install_dir>/boards/<board_name>/<example_type>/<application_name>/armgcc
For this guide, the exact path is:
<install_dir>/boards/evkmimxrt1170/demo_apps/hello_world/cm7/armgcc
This section describes steps to run a demo application using J-Link GDB Server application. To perform this exercise, make sure that either:
Note: Some hardware platforms require hardware modification in order to function correctly with an external debug interface.
Procedure to configure Freelink/LPC-Link2 interface with J-Link firmware:
After the J-Link interface is configured and connected, follow these steps to download and run the demo applications:
J11
) USB connector and the PC USB connector. If using a standalone J-Link debug pod, also connect it to the SWD/JTAG connector of the board. <install_dir>/boards/<board_name>/<example_type>/<application_name>/cm7/armgcc/debug
<install_dir>/boards/<board_name>/<example_type>/<application_name>/cm7/armgcc/release
For this guide, the path is:
<install_dir>/boards/evkmimxrt1170/demo_apps/hello_world/cm7/armgcc/debug
The hello_world application is now running, and a banner is displayed on the terminal. If this is not true, check your terminal settings and connections.
Refer to the Getting Started with MCUXpresso SDK for MIMXRT1170-EVK.pdf in the <SDK install folder>/docs folder from the SDK for additional information and instructions to build and run multicore example applications.
Something went wrong! Please try again.
The i.MX RT family supports a number of different boot sources, and includes the option for memory to be copied to an on-chip or external destination memory as well as Execute in Place (XIP) for some interfaces. Learn more about your choices and which one is best for your design.
Documents and Videos | Description |
---|---|
AN12108 How to Enable Boot from QSPI Flash | This document describes how to use Flashloader step by step to program a bootable image into the external storage device either by using Open SDA or MfgTool. |
AN12107 How to Enable Boot from Octal SPI Flash and SD Card | This document describes how to program a bootable image into the external storage device. |
MCUXpresso Secure Provisioning Tool A GUI-based application provided to simply generation and provisioning of bootable executables on NXP i.MX RT.
Community Resources for Booting Look for answers to your boot questions or submit new questions in our Community.
Documents and Videos | Description |
---|---|
AN12437 i.MX RT Series Performance Optimization | How to optimize the system performance running on different memory devices. |
AN12108 How to Enable Boot from QSPI Flash | This document describes how to use Flashloader step by step to program a bootable image into the external storage device either by using Open SDA or MfgTool. |
AN12107 How to Enable Boot from Octal SPI Flash and SD Card | This document describes how to program a bootable image into the external storage device. |
Developing Code Using the Adesto EcoXip Memory | Learn about the hardware and software requirements for configuring the NXP i.MX RT1050 EVKB board with an Adesto EcoXiP Flash device. |
AN12564 Implement Read While Write (RWW) on i.MX RT Series | How to implement RWW requirement on the i.MX RT series. |
AN12239 How to Enable HyperRAM with i.MX RT | How to use the HyperRAM with the i.MX RT MCU, including hardware connections, HyperRAM protocol, source code and performance. |
AN13028 Advanced HyperRAM/PSRAM Usage on i.MX RT | This application note describes the advanced usage of HyperRAM/PSRAM when used with FlexSPI on i.MX RT MCU, including FlexSPI prefetch function, HyperRAM/PSRAM refresh interval and HyperRAM devices supported. |
AN13204 i.MX RT1170 ECC Application | This document discusses the ECC application on memory, including TCM, Cache, OCRAM and external memory. |
AN12255 How to Use Flash Remapping Function | The i.MX RT1170 supports the flash remapping function, which allow users to remap flash address to FlexSPI interface. |
Several examples, demos and drivers are available within the SDK to help you get started. Some common examples for external memory are listed below.
How to use the FlexSPI driver with polling.
Path:
<SDK_PATH>/boards/evkbimxrt1170/driver_examples/flexspi/nor/polling_transfer
Multiple data transfer examples using EDMA.
Path:
<SDK_PATH>/boards/evkbimxrt1170/driver examples/flexspi/nor/edma_transfer
How to use the SEMC controller driver to initialize the external SDRAM chip.
Path:
<SDK_PATH>/boards/evkbimxrt1170/driver_examples/semc/sdram
How to use the external ECC controller (XECC) with FlexSPI or SDRAM
Path:
<SDK_PATH>/boards/evkbimxrt1170/driver examples/xecc
MCUXpresso Secure Provisioning Tool A GUI-based application provided to simply generation and provisioning of bootable executables on NXP i.MX RT.
The i.MX RT1170 is secure-by-design and supported by secure software driving the secure System-on-a-Chip (SoC).
Documents and Videos | Description |
---|---|
Secure Boot Webinar and demo | Using the latest NXP software and tools, you can integrate boot authentication and encrypted execution into your design based on i.MX RT10xx MCUs. Learn more about secure boot features and how the MCUXpresso Secure Provisioning Tool allows you to configure them. |
Realizing Today’s Security Requirements: Achieving End-To-End Security with a Crossover Processor | Learn about common shared security goals that IoT end and edge nodes should meet, as well as the steps, tools and procedures needed to achieve root of trust in end devices. |
AN13250 i.MX RT1170 Secure Boot Modes | Provides an overview of the secure boot modes available on the i.MX RT1170 family and how to enable them. |
AN13133 Secure JTAG for i.MX RT1170 | Describes the three JTAG security modes that are available on the i.MX RT series and how to use them on the i.MX RT1170 MCU. |
AN13078 How to Use Tamper Function | Tamper detection is a special mechanism to trigger violation and zeroize key information when the device encounters unauthorized opening or tampering. This application note explains how to use tamper function on i.MXRT1173. NOTE: The tamper detection feature is not supported on the i.MX RT1170-EVK. |
Several examples, demos and drivers are available within the SDK to help you get started. Some common examples related to security and integrity are listed below.
Program performs cryptographic algorithm benchmarking and testing. (Requires optional mbedTLS middleware package).
Path:
<SDK_PATH>/boards/evkbimxrt1170/mbedtls_examples/
Performs PUF enroll, start, generate key, set key and get key functions.
Path:
<SDK_PATH>/boards/evkbimxrt1170/driver_examples/puf
One-stop secure boot tool: NXP-MCUBootUtility A GUI tool specially designed for NXP MCU secure boot. It includes all the features of NXP’s official security enablement toolset with support for full graphical user interface operation.
MCUXpresso Secure Provisioning Tool A GUI-based application provided to simply generation and provisioning of bootable executables on NXP i.MX RT.
Documents and Videos | Description |
---|---|
Wired Communications Middleware for NXP Microcontrollers | Learn about wired communications libraries and examples provided through MCUXpresso SDK. |
CANopen in NXP’s MCUXpresso SDK | A demo combining different middleware components of the NXP MCUXpresso SDK using the i.MX RT1064 and LPC55S16 demo boards. |
CANopen and Embedded Wizard Demo featuring the i.MX RT 1064 and LPC55 | A demo combining different middleware components of the NXP MCUXpresso SDK using the i.MX RT1064 and LPC55S16 demo boards. |
AN12822 Emulating 8080 Bus with the FlexIO on RT1050 | How to use the FlexIO module to emulate the 8080 parallel bus and to drive a graphic TFT LCD with the 8080 bus interface. |
AN12679 Implement High-Speed RS-485 Application with i.MX RT Based on NXP SDK | How to implement RS-485 communication with NXP i.MX RT series EVK, and how to design software based on NXP MCUXpresso SDK. |
AN12103 Developing a Simple UVC Device Based on i.MX RT1050 | UVC is widely used for applications including desktop video cameras (webcams), digital camcorders and still-image cameras. This document describes how to develop a simple UVC device and introduces the hardware and software platforms of the demo application |
MCU Tech Minutes | Getting Started with CANopen and MCUXpresso | Learn how to download an SDK that includes EmSA's CANopen stacks and set up one manager and one device CANopen network. |
Employing TSN Over Ethernet to Enable Precision Motor Control through Operator Gesture | This demo shows the i.MX 8M Plus processor, i.MX RT1170 MCU and Layerscape LS1028A using different protocols as well as custom motor control messages over TSN Ethernet in a complex industrial system. |
AN13114 Enable More USB Examples on M4 Core for RT1170 | RT1170 works with M7 and M4, on which all USB examples can run. However, all USB examples in the release package are enabled on M7. This document describes how to migrate USB examples from M7 to M4 with different toolchains |
Several examples, demos and drivers are available within the SDK to help you get started. Some common examples related to wired communications are listed below.
Implements a minimal CANopen Manager and CiA 401 generic I/O device. (Requires optional CANopen middleware package).
Path:
<SDK_PATH>/boards/evkbimxrt1170/canopen_examples/
Various demos and examples for the lwIP TCP/IP stack, which uses the ICMP protocol. (rRquires optional lwIP middleware package).
Path:
<SDK_PATH>/boards/evkbimxrt1170/lwip_examples/
A number of USB examples for host and device operation exist within the SDK. (Requires optional USB Host, Device, OTG stack middleware package).
Path:
<SDK_PATH>/boards/evkbimxrt1170/usb_examples/
Accelerate Development of Robust Network Communications with CANopen and CANopen FD NXP has partnered with EmSA to offer CANopen as an enablish software technology. Fully integrated CANopen Libraries based on MicroCANopen Plus v7.0 are available in the MCUXpresso SDK.
Documents and Videos | Description |
---|---|
NXP Wireless Connectivity | Our portfolio of low-power, cost-effective wireless solutions address many monitoring and control applications for the Internet of Things. |
Cloud Connectivity on NXP Microcontrollers | Integrated support for cloud services including Amazon Web Services, Microsoft Azure and Google Cloud IoT. |
Getting Started with NXP Wi-Fi modules using i.MX RT platform | Let's take your Wi-Fi module for a test drive. This guide uses the Wi-Fi modules and i.MX RT platforms! |
AN12257 IoT Device Secure Connection with LoRa | This document explains how to establish IoT secure connection with LoRa between gateway and end devices. |
Several examples, demos and drivers are available within the SDK to help you get started. Some common examples related to wired communications are listed below.
Amazon FreeRTOS Qualification (AFQ), device configuration, AWS Greengrass discovery, remote control by Android mobile application and shadow lightbulb demos.
Path:
<SDK_PATH>/boards/evkbimxrt1170/aws_examples
A small demo of the high-performance ThreadX kernel.
Path:
<SDK_PATH>/boards/evkbimxrt1170/azure_rtos_examples/threadx_demo
CLI support usage example, iPerf network performance measurement, Wi-Fi test mode example and Wi-Fi configuration utility demos.
Path:
<SDK_PATH>/boards/evkbimxrt1170/wifi_examples/
HOMEKIT-SDK The HomeKit Software Development Kit (SDK) from NXP offers support for home automation applications using Apple HomeKit technology, delivering great performance, advanced security and supporting all connectivity options; Bluetooth Smart®(Bluetooth Low Energy), Wi-Fi, Ethernet and remote access over iCloud.
Documents and Videos | Description |
---|---|
AN13264 i.MX RT1170 Dual Core Application | Introduces the dual-core application on i.MX RT1170, including boot, MU/SEMA4/RDC/XRDC2/Shared memory and dual-core debug in a different tool chain. |
How to use JLINK to debug RT1170 dual core | The dual core i.MX RT117x devices have one Cortex-M7 core and one Cortex-M4 core that can be debugged simultaneously via JLINK if some additional setting changes are made. |
Several examples, demos and drivers are available within the SDK to help you get started. A common examples related to power management is listed below.
How to use the FlexSPI driver with polling.
Path:
<SDK_PATH>/boards/evkbimxrt1170/multicore_examples
Demonstrates the use of power modes in the KSDK for bare metal or RTOS.
Path:
<SDK_PATH>/boards/evkbimxrt1170/demo_apps/power_mode_switch
Power management includes device-specific techniques and information on power management and low-power optimization.
Documents and Videos | Description |
---|---|
AN13116 Entering STBY mode on a single-core RT1170 | This application note outline steps to enter the STBY mode on a single core RT1170 and simulate a single-core state on RT1170 EVK. |
AN13104 Debug and Application for RT1170 Clock and Low Power Feature | This application note introduces not only clock and low-power features in RT1170, but also some debug and application skills when developing a low-power use case. |
AN13148 i.MX RT1170 Low-Power Modes | This document describes the i.MX RT1170 power architecture design, clock architecture, and how the low-power modes can be used and configured. |
Several examples, demos and drivers are available within the SDK to help you get started. A common examples related to power management is listed below.
Demonstrates the use of power modes in the KSDK for bare metal or RTOS.
Path:
<SDK_PATH>/boards/evkbimxrt1170/demo_apps/power_mode_switch
Documents and Videos | Description |
---|---|
Audio Software on NXP Microcontrollers | Middleware, example applications, MCUXpresso Config tools and partner solutions for advanced audio applications. |
AN12090 Using Multi-Channel Feature of SAI | This document introduces the technology of a 7.1 surround sound system, including SAI and FLAC, and provides guidance on how to use the multi-channel SAI feature to develop applications running in a correct high-performance way. |
Several examples, demos and drivers are available within the SDK to help you get started. Some common examples related to motor control are listed below.
Demonstrates complicated digital audio playback and record case.
Path:
<SDK_PATH>/boards/evkbimxrt1170/demo_apps/sai
Demonstrates how to use the asynchronous sample rate converter module.
Path:
<SDK_PATH>/boards/evkbimxrt1170/driver_examples/asrc
Demonstrates how to use spdif driver with EDMA and interrupt.
Path:
<SDK_PATH>/boards/evkbimxrt1170/driver_examples/spdif
Multiple EDMA and interrupt examples.
Path:
<SDK_PATH>/boards/evkbimxrt1170/driver_examples/pdm
The LCD panel that works with the IMIXRT1170EVK and is used in the MCUXpresso SDK graphics examples is the RK055HDMIPI4M.
Documents and Videos | Description |
---|---|
Graphics for NXP Microcontrollers | Graphics libraries and tools from multiple partners for developing embedded GUIs of all levels of complexity. |
Cost-Effective Embedded HMI Solutions with i.MX RT1170 | Drive down your costs while combining safety and modern UX by developing with the i.MX RT1170 crossover MCU and "Qt for MCUs". |
Design Your Next Graphical UI for Industrial HMI Applications Using NXP’s i.MX RT1170 MCU, GUI Guider and LVGL | Learn more about the i.MX RT1170 MCU and see how LVGL and GUI Guider make it easy to design your next embedded GUI. |
Implementing Graphics in Real-time Industrial HMI Systems with NXP MCUs and Embedded Wizard | NXP has partnered with TARA Systems to offer Embedded Wizard as an Enabling Software Technology. |
Getting Started with Embedded Wizard and MCUXpresso | Learn how to download an SDK that includes Embedded Wizard and get an example project up and running on your device. |
Creating Graphics on the i.MX RT1060 | Learn how to develop graphics on the i.MX RT, which supports product designs with advanced multimedia for GUI and enhanced human machine interface (HMI) experience. |
Implementing Graphics in Real Time Industrial HMI Systems with i.MX RT10xx MCUs and Crank Storyboard | NXP has partnered with Crank Software to offer Storyboard as an Enabling Software Technology. |
Simplifying the Creation of Stunning GUIs | Introducing Embedded Wizard in the MCUXpresso SDK. |
AN12302 i.MX RT eLCDIF RGB Mode Use Case | An example using the enhanced Liquid Crystal Display Interface (eLCDIF) on the MIMXRT1050-EVKB board. |
AN13075 i.MX RT1170 Heterogeneous Graphics Pipeline | A brief overview of the graphics engines on the i.MX RT1170 as well as how to use them independently and in unison. |
AN12940 Use Case of RT1170 LCD Display System based on MIPI DSI | How to use the MIPI DSI Host Controller and LCDIFv2 Controller to drive a DSI-compliant LCD panel on i.MX RT1170. |
Several examples, demos and drivers are available within the SDK to help you get started. Some common examples related to display and graphics are listed below.
Demonstrate how to use emWin library to render text and graphical widgets. (Requires optional emWin middleware package).
Path:
<SDK_PATH>/boards/boards/evkbimxrt1170/emwin_examples
Reads the JPEG pictures from the SD card, decodes them, and shows them in the LCD panel one by one (Requires optional JPEG library middleware package).
Path:
<SDK_PATH>/boards/evkbimxrt1170/jpeg_examples
Demonstrates littlevgl widgets (Requires optional LVGL middleware package).
Path:
<SDK_PATH>/boards/evkbimxrt1170/vlittlevgl_examples
Demonstrates OpenVG graphics library (Requires optional openvg middleware package).
Path:
<SDK_PATH>/boards/evkbimxrt1170/openvg_examples
Demonstrates VGlite graphics library (Requires optional vglite middleware package).
Path:
<SDK_PATH>/boards/evkbimxrt1170/vglite_examples
LVGL Open-Source Graphics Library LVGL is a free and open-source embedded graphic library with features that enable you to create embedded GUIs with intuitive graphical elements, beautiful visual effects and a low memory footprint.
GUI Guider A user-friendly graphical user interface development tool from NXP that enables the rapid development of high-quality displays with the open-source LVGL graphics library.
The LCD panel that works with the IMIXRT1170EVK and is used in the MCUXpresso SDK graphics examples is the RK043FN01H-CT.
Documents and Videos | Description |
---|---|
AN12110 Developing a Camera Application with i.MX RT Series | How to develop an HD camera application with the NXP i.MX RT1050 processor. |
AN13205 Development of H.264 Video Encode on RT Series | How to develop an H264 video encoder application with the i.MX RT1170 processor. |
Several examples, demos and drivers are available within the SDK to help you get started. Some common examples related to camera interfaces are listed below.
This project shows how to receive the camera data using CSI driver for RGB data.
Path:
<SDK_PATH>/boards/evkbimx1170/driver_examples/csi/mipi_rgb
This project shows how to receive the camera data using CSI driver with YUV format data.
Path:
<SDK_PATH>/boards/evkbimx1170/driver_examples/csi/mipi_yuv
Documents and Videos | Description |
---|---|
AN13065 Gender Voice Recognition with TensorFlow Lite Inference | This document describes the steps to train the TensorFlow model on Gender voice audio samples and classification. |
Clarinox Democratization of BT/BLE/Wi-Fi Technologies on NXP i.MX RT1170 MCUs for IoT Gateways | The i.MX RT1170 MCU is a perfect platform to run complex Bluetooth and Wi-Fi use cases such as the IoT gateway. |
Machine learning (ML) typically encompasses applications where classification, recognition and prediction of man-made abstractions are desired. Examples include Image Recognition, Gesture Recognition, Anomaly Detection, Speech-to-Text, Text-to-Speech, ASR, Scene Recognition and many more.
Documents and Videos | Description |
---|---|
eIQ® ML Software Development Environment | Enables the use of ML algorithms on NXP MCUs, i.MX RT crossover MCUs and i.MX family SoCs. eIQ software includes inference engines, neural network compilers and optimized libraries. |
Getting Started with eIQ on i.MX RT | How to download eIQ Machine Learning software enablement and run it with MCUXpresso IDE, VS Code, IAR or Keil MDK. |
eIQ Fact Sheet | Machine learning software for NXP i.MX and MCUs – libraries, example applications and inference engines. |
eIQ Glow Lab for i.MX RT | Learn how to use the Glow neural network compiler tool by running a handwritten digit recognition model example. A step-by-step video covering this lab is also available below. |
eIQ Toolkit and DeepViewRT Labs for i.MX RT | Learn how to use eIQ Toolkit to generate your own image classification and object detection models and deploy them onto i.MX RT devices. Also learn about the eIQ DeepViewRT inference engine. |
eIQ TensorFlow Lite for Microcontrollers Lab for i.MX RT | Learn how to run your own TFLite model on i.MX RT microcontrollers using the TensorFlow Lite for Microcontrollers (TFLM) inference engine. |
Application Software Pack: ML-Based System State Monitor | This ML application software pack is designed to show how to create a fan vibration state monitoring solution and can also be used for other time-series anomaly detection use cases. |
AN13001 Glow Memory Analysis | How to understand the Glow memory information generated by the Glow compiler and calculate the memory required for a particular model. This compiler can then be used to determine the minimum memory size that is needed to run the model. |
AN12766 Anomaly Detection with eIQ using K-Means clustering in Tensor Flow Lite | Step by step instruction to enable a machine condition monitoring application using anomaly detection. |
AN12781 Caffe Model Development on MNIST Dataset with CMSIS-NN Library | Describes the process to train a Caffe model on MNIST dataset for digit classification. The trained Caffe model is converted to a source file that can run on i.MX RT platforms. |
MCU Tech Minute: Multistage ML with the Coral Development Board | To enable truly battery operated ML, Coral introduces a two part "wake-to-run" ML workflow that takes advantage of the capabilities offered by NXP's i.MX RT1176 MCU, and pairs them with the Coral Edge TPU. |
Several examples, demos and drivers are available within the SDK to help you get started. Some common examples related to machine learning are listed below.
Several examples demonstrating machine learning applications using TensorFlow Lite for Microcontrollers, DeepViewRT and Glow (Requires optional eIQ middleware package).
Path:
<SDK_PATH>/boards/evkbimxrt1170/eiq_examples
Motor control is a complicated and advanced topic, with a wide range of intricacies and pitfalls that depend on the number of motors, motor type and sensored or sensorless motor drivers.
NXP has a number of ready-to-use motor control algorithms (middleware), and the best way to get started is with the FreeMaster examples included in the MCUXpresso SDK. These examples utilize the FreeMASTER Run-Time Debugging Tool , a user-friendly real-time debug monitor and data visualization tool that enables runtime configuration and tuning of embedded software applications.
FreeMASTER supports non-intrusive monitoring of variables on a running system and can display multiple variables on oscilloscope-like displays as standard widgets (gauges, sliders and more) or as data in text form, offering simple-to-use data recorders. It can link with HTML, MATLAB® or Excel to other scriptable frameworks or even popular visual programming tools like Node-RED .
Documents and Videos | Description |
---|---|
Get Your Motor Spinning with i.MX RT | This presentation covers the MCU requirements, motor control basics and framework to spin a BLDC, PMSM or ACIM motor and how to implement motor control on the i.MX RT. |
Employing TSN Over Ethernet to Enable Precision Motor Control through Operator Gesture | This demo shows the i.MX 8M Plus processor, i.MX RT1170 MCU and Layerscape LS1028A using different protocols as well as custom motor control messages over TSN Ethernet in a complex industrial system. |
AN12214 PMSM Field-Oriented Control on MIMXRT10xx EVK | Describes the implementation of the sensor and sensorless speed and position motor control software for 3-phase Permanent Magnet Synchronous Motors (PMSM). |
PMSM Field-Oriented Control on MIMXRT10xx EVK User’s Guide | Step-by-step guide on how to open, compile, debug and run Permanent Magnet Synchronous Motor (PMSM) projects in most common IDEs, as well as how to turn the NXP Freedom PMSM power stage and the i.MX RT10xx evaluation kit into a complete motor control reference design. |
AN12659 NXP quad motor-control development platform HW | Describes the NXP quad motor-control development platform modular architecture and provides a detailed hardware description of the different components. |
AN12200 Dual FOC Servo Motor Control on i.MX RT | Describes the dual servo demo with the NXP i.MX RT1020 processor. You can use it as a reference for motor control application developing based on other i.MX RT products. |
FreeMASTER How To | A starting guide for engineers using FreeMASTER tool. |
FreeMASTER 3.0 Installation Guide | This article will walk you through the installation process of FreeMASTER 3.0. |
FreeMASTER Four-Part Webinar Series | On-demand training provides an overview of the FreeMASTER software, its features, capabilities, available examples, application use cases and how to easily get started. |
Several examples, demos and drivers are available within the SDK to help you get started. Some common examples related to motor control are listed below. Note that all examples require the optional motor control middleware package.
AC induction motor middleware.
Path:
<SDK_PATH>/middleware /motor_control/acim
Brushless DC electric motor middleware.
Path:
<SDK_PATH>/middleware/motor_control/bldc
Freemaster middleware for motor control examples.
Path:
<SDK_PATH>/middleware/motor_control/freemaster
Permanent magnet synchronous motor middleware.
Path:
<SDK_PATH>/middleware/motor_control/pmsm
The most recent versions of MCUXpresso IDE count with a terminal emulation application. This tool can be used to display information sent from your NXP development platform's virtual serial port.
Verify that the connection is open. If connected, MCUXpresso IDE will look like the figure below at the Terminal view.
You're ready to go
Tera Term is a very popular open source terminal emulation application. This program can be used to display information sent from your NXP development platform's virtual serial port.
DownloadPuTTY is a popular terminal emulation application. This program can be used to display information sent from your NXP development platform's virtual serial port.
Download
To learn what to do next, find your issue below. If you still need help, contact NXP Support.
Basic Application Development Using MCUXpresso IDE and MCUXpresso Config Tools – This three-part video series covers the basic interactions between the MCUXpresso IDE and Config Tools when working with either an imported SDK example project or creating a new one.
MCU Tech Minutes- Key Features and Benefits of the i.MX RT series – Short video presentations introduce some of the key features and benefits of the i.MX RT series.
MCU Minutes: Introducing the i.MX RT1170 Crossover MCU - NXP offers breakthrough performance with the 1GHz i.MX RT1170.
Architecture and Features of the i.MX RT1170 MCU family - The i.MX RT1170 family is the most powerful of the Crossover microcontrollers, designed for Machine Learning, IoT, industrial automation, multimedia and audio applications.
Graphics Applications with the i.MX RT1170 Family of MCUs – Learn about hardware resources for graphic applications, middleware libraries for the i.MX RT1170 and watch an Embedded Wizard demo.
i.MX RT1170 Training - Full list of on-demand training, how-to videos and webinars from NXP about this product.
Connect with other engineers and get expert advice on designing with the i.MX RT1170 on one of our community sites.
Installing Software for MIMXRT1170-EVK
Jump Start Your Design with the MCUXpresso SDK
Get Your Toolchain
MCUXpresso Config Tools
PC Configuration
Serial Terminal
Build and Run an SDK Multicore Demo on the MIMXRT1170-EVK
Explore the MCUXpresso SDK Example Code
Building and debugging MCUXpresso SDK Examples