1
Get Started2
Know the Board3
Configure Hardware4
Install SoftwareSign in to save your progress. Don't have an account? Create one.

The NXP analog product development boards provide an easy-to-use platform for evaluating NXP products. The boards support a range of analog, mixed-signal and power solutions. They incorporate monolithic integrated circuits and system-in-package devices that use proven high-volume technology. NXP products offer longer battery life, a smaller form factor, reduced component counts, lower cost and improved performance in powering state-of-the-art systems.
This page will guide you through learning about how to set up the FRDM-PF1510EVM board.
The FRDM-PF1510EVM contents include:
Something went wrong! Please try again.
This kit requires the following items:
Something went wrong! Please try again.
The kit requires the following to function properly with the software:
Something went wrong! Please try again.
| Device | Description | Features |
|---|---|---|
| PF1510 | Power management integrated circuit (PMIC) for i.MX 7ULP, 6SL, 6UL, 6ULL, and 6SX processors |
|
Something went wrong! Please try again.
The FRDM-PF1510EVM boards serve as an evaluation platform that allows users to test and demo designs that incorporate the PF1510 PMIC. The evaluation board contains a pre-configured MC32PF1510A4EP device and provides numerous jumpers and test points that allow users to tailor the evaluation to their needs. The kit comes with an FRDM-KL25Z already mounted and loaded with compatible microcode. The primary function of the FRDM-KL25Z is to control communication between the evaluation board and a PC.
Something went wrong! Please try again.
The FRDM-KL25Z evaluation board was chosen specifically to work with the FRDM-PF1510EVM kit because of its low cost and features. The FRDM-KL25Z board uses the USB, built-in LEDs, and I/O ports available with NXPs Kinetis KL2x family of microcontrollers.
The FRDM-PF1510EVM connects to the FRDM-KL25Z using the four-dual row Arduino R3 connectors on the bottom of the board.
Suggested equipment's needed for test:
Something went wrong! Please try again.
Connect the mini-USB cable from a PC to the KL25Z USB port on the FRDM-KL25Z board. Connect the other end of the cable to a host computer.
Something went wrong! Please try again.
Download and run SW for the FRDM-PF1510EVM with the next step.
Something went wrong! Please try again.
PF1510_x_Bx.jar)Main log window indicate a connection.
Something went wrong! Please try again.
For PF1510 is located at PF1510.
The overview tab provides an overview of the device, product features, a description of the kit contents, a list of (and links to) supported devices, list of (and links to) any related products and a Get Started section.
In addition to our PF1510 Power Management Integrated Circuit (PMIC) for low power application processors page you may also want to visit:
Connect with other engineers and get expert advice on designing with the FRDM-PF1510EVM on our community site.